• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Reverse-polarity Protection Comparison: Diode vs. PFET vs. a Smart Diode Solution

    • SSZTBS3 December   2015 LM74610-Q1

       

  • CONTENTS
  • SEARCH
  • Reverse-polarity Protection Comparison: Diode vs. PFET vs. a Smart Diode Solution
  1.   1
  2.   2
    1.     3
    2.     1) Thermals
    3.     5
    4.     2) Dynamic Reverse-Polarity
    5.     3) Voltage Interruption
    6.     4) Power Line Disturbance/Superimposed AC Voltage
    7.     5) Quiescent Current
    8.     6) Leakage Current
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Reverse-polarity Protection Comparison: Diode vs. PFET vs. a Smart Diode Solution

Mathew Jacob

When you fly on an airline, you’ll occasionally hear “Thank you for flying with X; we know you have many choices when you fly.” Similarly, engineers have many choices when it comes to picking reverse-polarity solutions. Some of the choices include diode, P-channel field effect transistor (PFET), and TI’s LM74610-Q1 plus N-channel field effect transistor (NFET) (called a smart diode solution). In this post, I’ll highlight some key aspects of all three solutions with regards to automotive applications.

I will pick a couple of application specific parameters for comparison purposes: thermals, dynamic reverse polarity, voltage interruption, continuous power-line disturbance and quiescent current (Iq), and leakage current.

1) Thermals

Thermals are usually the deciding factor when choosing between a diode solution and a FET solution. Figure 1 shows the board I used to compare. The smart diode is the “coolest” solution and shows the lowest temperature rise seen in Figure 2. The temperature rise of PFETs is much higher if the input voltage drops to 6V (similar to start-stop voltages), since the Rdson increases dramatically at lower input voltages. Of course, take one look at the diode temperature and you’ll say “ouch.”

GUID-C0654A20-9C2A-4028-870E-2220ADB40B84-low.png Figure 1 Board Used for Comparison of Thermal
GUID-D292B4C4-B0A0-497D-BBA5-3F023AA22501-low.png GUID-9DBB2D47-DCD7-4FC8-BAD8-0FA71E60D333-low.png GUID-1984DD25-6E79-4A9A-AECD-C361ED21E1B5-low.png Figure 2 Thermal Measurements with 10A Current and vIN = 6V

2) Dynamic Reverse-Polarity

The dynamic reverse-polarity requirement comes primarily from standards testing requirements such as ISO7637 and OEM-specific requirements. You can use diodes, PFETs and NFETs but their performance is related to other component values. Figure 3 illustrates how diodes and a smart diode solution are very similar in performance, whereas with the PFET solution the voltage goes negative (depending on the output capacitor used). Due to the slow response time, you will need bigger output capacitors, as shown in Figure 4.

GUID-A076A972-CC40-4DEF-901F-8DE5D6A95DE3-low.png GUID-95229E53-5F1A-43BF-B5AB-191089218360-low.png GUID-A69CAAC4-7A28-4A05-9092-003456FD8B5E-low.png Figure 3 Dynamic Input Voltage Reversal, 12V to -20V, Cout = 4.7µF, Io = 0.1A
GUID-962EE377-5B2B-4D10-A6E2-8EC7F169334F-low.png Figure 4 Dynamic Input-voltage Reversal, 12V to -20V, Cout = 2200µF, Io = 0.1A

3) Voltage Interruption

The voltage interruption requirement comes specifically from OEM specifications and is meant to simulate loose contact at the battery terminal or module wiring. As shown in Figure 5, diodes and the smart diode solution are very similar in performance, whereas with the PFET solution the voltage dips very low. The name of the game is to keep the output voltage high for small voltage interruptions. In the case of interruptions, reverse current flows from the output capacitors back into the input. In the case of diodes and the smart diode solution, the reverse current is blocked. The PFETs allow reverse current back and hence deplete the output capacitor. In practice, this means less hold-up time for an interrupt event.

GUID-C29A46A3-2D74-4051-B8EA-CEB6E01C5030-low.png GUID-A17BA86E-5AA8-40D0-A713-BA571F769A64-low.png GUID-52B2CE1E-DA9C-42B5-8ABB-CAF4D47FD699-low.png Figure 5 Voltage Interruption, 12V to 0V, T = 2ms, Cout = 100µF, Io = 0.1A

4) Power Line Disturbance/Superimposed AC Voltage

The continuous power-line disturbance requirement comes from the fact that alternators create noise/AC ripple on DC voltages. The AC ripple at different frequencies can cause high ripple current if reverse currents are not blocked. The repercussions of high ripple current are lower reliability for the electrolytic capacitors and higher temperature rise. Figure 6 shows the difference in ripple currents: 5KHz for a diode, 7A for the smart diode solution and 25A for the PFET.

GUID-03AB7478-3F39-499A-8135-860CA2FA8FD7-low.png GUID-2182A61E-748D-47E1-85F9-9C7BE9173481-low.png GUID-BDBDFCC9-8FF9-4F4A-91EF-F54560C489B7-low.png Figure 6 Superimposed AC Voltage, 2V Peak to Peak at 5KHz and Io = 3A

5) Quiescent Current

Quiescent current is a big, big deal for automotive applications. A complete module is allowed a maximum 100µA for standby currents (Iq). The smart diode solution mimics a diode with zero Iq. With a PFET solution, the Iq can be higher than 100µA unless you use additional circuitry to turn off the gate-drive bias.

6) Leakage Current

Leakage currents are often overlooked in most single input applications. How it plays a role in real-world scenarios is sometimes confusing. Let’s take an ORing application with two diodes. If one of the inputs turns off, you would expect the voltage at this point to be zero. Due to some leakage current, however, the voltage from the output leaks back into the input and you see some voltage there. If you draw more current from the input than the leakage spec, the voltage will drop to zero. Schottky diodes have low leakage currents at 25°C but go much higher at high temperatures. For example, a MBR1545 diode has 1.5µA of leakage at 25°C and 1mA at 125°C. PFET solutions have infinite leakage, since they allow current to flow back into the input if the FET is not turned off. In comparison, the smart diode solution has leakage of 60µA at 25°C and 110µA at 125°C.

After making all of these comparisons, it can be seen that the smart diode solution (a LM74610-Q1 plus NFET) is superior to both diodes and PFET-based schemes used in reverse-polarity designs for automotive applications. As I had mentioned in the beginning, when you are ready to dive into your next design of a reverse polarity solution, I hope you will do a test drive of the smart diode solution considering the various advantages it brings to the table.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale