• Menu
  • Product
  • Email
  • PDF
  • Order now
  • LDO Basics: Current Limit

    • SSZTA58 May   2017 TLV717P , TPS7A16

       

  • CONTENTS
  • SEARCH
  • LDO Basics: Current Limit
  1.   1
  2.   2
    1.     3
    2.     What Is Current Limiting/how Does It Work?
    3.     Brick-wall Current Limiting
    4.     Foldback Current Limit
    5.     Additional Resources:
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

LDO Basics: Current Limit

Jose Gonzalez Torres

The key goal of DC power management is to provide a regulated, steady voltage for the slew of electronic content present in any system. This is particularly true for low-dropout regulators (LDOs), as they can achieve a regulated voltage while supplying current as needed.

There are external conditions and scenarios where an LDO might experience an unexpected high current draw. This high current will harm most electronic systems as well as the host power-management circuit if the current is transmitted to the other electronics being powered. Selecting an LDO with internal protection from short circuits and current limiting can help prevent this harmful effect and provide additional protection when designing the overall power management.

What Is Current Limiting/how Does It Work?

Current limit in an LDO is defined by establishing an upper boundary for the current supplied. Unlike a constant current source, LDOs supply current on demand but can also control the total power regulated. Current limiting is achieved through internal circuitry controlling the output stage transistors inside the LDO. See Figure 1. This is a classic current-limit circuit for an LDO and is commonly referred to as a “brick-wall” current limit due to its abrupt current stop once the limit is reached. In this internal circuit, the LDO measures the output voltage for feedback but also measures a scaled mirror of the output current against the internal reference (IREF).

GUID-DE16B715-F45E-4BEC-9022-71E3CACF0967-low.png Figure 1 A Current-limiting Internal LDO Structure

Brick-wall Current Limiting

In a brick-wall current limit, the upper boundary is defined and the LDO supplies current incrementally until the limit current limit is reached. Once the current limit is exceeded, the output voltage is not regulated and is determined by the resistance for the load circuitry (RLOAD) and the output current limit (ILIMIT) (Figure 1

GUID-7FCD6870-DF16-4432-8062-1E5C07098C69-low.png Figure 2 (1)

The pass transistor will continue this operation and dissipate power, as long as the thermal resistance (θJA) allows for healthy power dissipation where the junction temperature is within acceptable limits (TJ < 125°C). Once VOUT goes too low and the thermal limit is reached, thermal shutdown will turn off the device in order to protect it from permanent damage. Once the device has cooled, it will turn back on and regulation can proceed. This is particularly important in cases where a short circuit may present itself, as the LDO will proceed to regulate VOUT to 0V.

For example, TI’s TPS7A16 can limit high current outputs in wide voltage conditions. Figure 3 shows an example behavior of the current-limiting function in 30V input conditions. As you can see, once the current limit is surpassed, the LDO continues to supply at the limit, but it will no longer regulate VOUT to 3.3V. Once the thermal limit is surpassed at 105mA, thermal shutdown kicks in.

This current-limiting function is helpful for charging nickel-cadmium and nickel-metal hydride single-cell batteries, as both require a constant current supply. An LDO like the TPS7A16 can help maintain a constant current at the limit (ILIMIT) as the battery voltage changes while the battery is charging.

GUID-AB519D3C-9513-4AF5-A541-1FBB5B2F8F88-low.png Figure 3 TPS7A16 Brick-wall Current Limiting (30VIN, 3.3VVIN, VSON at 25°C)

Foldback Current Limit

Foldback current limit is very similar to the standard upper-boundary limit. But the main goal of foldback current is to limit the total power dissipation, keeping the output transistor within its safe power-dissipation limit by reducing the output current limit linearly while VOUT decreases and VIN remains steady.

Devices like the TLV717P feature foldback current limiting and benefit from it, due to being predominantly offered in very small packages with higher thermal impedance. If you look at the behavior of the TLV717P’s output current limit, as shown in Figure 4, you can see that the maximum power dissipation allowed at 25°C is 150mW, as VIN is specified as VOUT + 0.5V. After the current limit is exceeded and VOUT begins to reduce (assuming a constant RLOAD), both IOUT and the power dissipation reduce. This adds a bit of complexity for non-ohmic devices that draw a constant current and could trigger a lockout condition in which the powered device continues to reduce VOUT and the LDO continues to reduce IOUT.

GUID-25557C30-75DF-4068-86F6-8F5CD67A4F9F-low.png Figure 4 TLV717P Output Current Limit vs. VOUT

Whenever harmful conditions may be present such as short circuits or overloading, it is important to prevent the transmission of this effect to other sensitive electronics. Protected LDOs can provide a wide range of functionality that can make any design much more robust. Read more blog posts on the basics of LDO design.

Additional Resources:

  • Watch: Engineer it: Measuring thermals- How hot is your LDO?
  • Design: Contactless position sensor for variable speed trigger switch with <65μA consumption reference design

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2024, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale