The LAUNCHXL-F2800137 is a low-cost development board for the Texas Instruments C2000™ Real-Time Microcontroller series of F280013x devices. The LAUNCHXL-F2800137 is designed around the TMS320F2800137 real-time MCU and highlights the control, analog, and communications peripherals, as well as the integrated nonvolatile memory. The LaunchPad™ Development Kit also features two independent BoosterPack™ XL expansion connectors (80-pins), on-board Controller Area Network (CAN) transceiver, one 5-V encoder interface (eQEP) connector, power-domain isolation, and an on-board XDS110 debug probe.
Figure 1-1 highlights the key features of the F280013x LaunchPad.
Figure 1-1 F280013x LaunchPad™ Board OverviewC2000™, LaunchPad™, BoosterPack™, and Code Composer Studio™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.