The F2800157 controlCARD (TMDSCNCD2800157) from Texas Instruments (TI) provides a great way to learn and experiment with the F280015x devices. The F280015x device is a member of TI’s C2000™ family of microcontrollers (MCUs). This 120-pin controlCARD is intended to provide a well-filtered robust design that is capable of working in most environments. This document provides the hardware details of the F2800157 controlCARD and explains the functions, locations of jumpers, and connectors present on the board.
C2000™ and Code Composer Studio™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
Figure 1-1 F2800157 controlCARDEach controlCARD comes with a Hardware Developer’s Kit, which is a full set of files necessary to evaluate and develop with a C2000 device. These files include:
The Hardware Developer's Kit for the controlCARD can be found in the C2000Ware at the following location:
-
<install
directory>\c2000\C2000Ware_x_xx_xx_xx\boards\controlCARDs\TMDSCNCD2800157\Rx_x
The controlCARD can be completely powered and operated from the USB-C connector. In this stand-alone mode the on-board isolated power supply will provide power to the F2800157 device; no additional hardware is required. Optionally, an external 5 V supply can be provided to power the F2800157 device. For a detailed explanation of the hardware configuration, see Section 4.3.
When the controlCARD is used in a high-voltage setup, it is the user’s responsibility to confirm that the voltages and isolation requirements are identified and understood prior to energizing the board or simulation. When energized, the controlCARD or components connected to the controlCARD cannot be touched. Furthermore, the capacitor C7:A must be removed to minimize the possibility of leakage current flowing across the isolation barrier of the controlCARD.