The power estimation spreadsheet provides power consumption estimates based on measured and simulated data; the estimates are provided as is and are not verified within a specified precision. Power consumption depends on electrical parameters, silicon process variations, environmental conditions, and use cases running on the processor during operation. Actual power consumption must be verified in the real system. This tool is meant for estimating power consumption during realistic operating modes and is not intended for power supply sizing. This power estimation spreadsheet is preliminary and subject to change. The spreadsheet mentioned in this document can be downloaded from AM62D-PET-CALC.
Ethernet® is a registered trademark of Xerox Corporation.
All trademarks are the property of their respective owners.
The power estimation tool is a design resource to assist with the development process. This tool consists of a spreadsheet that helps estimate the SoC power consumption in active state based on specific application use cases. The SoC resource utilization, speed, IO configuration and peripherals must be represented accurately in the PET inputs for the tool to be effective. The usage of the spreadsheet is explained further in the document.