• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Achieving Faster Secure Boot Time on AM26x Devices

    • SPRADM8 November   2024 AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

       

  • CONTENTS
  • SEARCH
  • Achieving Faster Secure Boot Time on AM26x Devices
  1.   1
  2.   2
  3.   Trademarks
  4. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Application Brief

Achieving Faster Secure Boot Time on AM26x Devices

As cybersecurity regulations are becoming widely enforced to make sure that the devices in Automotive and Industrial domains are safe from malicious attacks. The TI SoCs are being widely used in these domain. The TI AM26x SoCs is a real time capable device with multitude of features like Real time ARM R cores, advance sensing, precise control, gigabit connectivity and dedicated components that enables design of systems with cyber security and functional safety requirements. In this document we can be looking at secure boot enhancements and performance benchmarks for AM26x SoC family.

Introduction

The advantage an external flash device offers is flexible NVM memory size for storing application software without upgrading or changing the existing SoC, when challenged with memory constraints. On the flip side, if proper security measures are not in place,then an unauthorized program can be loaded into the memory. The unauthorized program can render the system to be inoperable, expose sensitive and confidential data to the malicious agent, and in cases, can have life threatening consequences, damages to reputation, and legal liabilities.

AM26x (AM263x and AM263Px) device family supports securely booting the user code without compromising on the authenticity and confidentiality of user information like code, data, keys, and so on. AM26x microcontroller family support interfaces like OSPI and QSPI which allow integration of external flash devices and also providing secure boot feature. Thus enabling the user with the flexibility of external flash technology while maintaining the security of the system.

Cryptographic Strengths of AM26 Secure Boot include:

  • RSA-PKCS1-v1_5 and SHA512 digest is used for verification of the certificate
  • SHA512 is used to maintain the integrity of the bootloader Image.
  • AES-CBC-256 is used to decrypt the image to maintain the confidentiality of the image.

Fast Boot Techniques

The following sections include information about different boot optimization techniques used to improve boot time performance.

Flash Clock, Configuration, and DMA integration

AM26x device family does not have an internal non-volatile memory for code execution and relies heavily on internal volatile memories (TCM and SRAM). Like many other advance SOCs, AM26x devices also have multi stage boot architecture. During the ROM bootloader(RBL) the copies the Secondary bootloader(SBL) image from external flash (over SPI) into the internal memory. In SPI protocol, the data speed (bps) is directly proportional to the frequency (Hz) at which SPI peripheral is clocked. As per JEDEC xSPI standard configuring the OSPI controller to support higher modes enables faster data transfers. Hence, a higher SPI clock and higher configuration can lead to better performance.

Table 1 Flash Controller Comparison on AM26x Devices
AM263x AM263Px
Maximum Flash Clock 80MHz 133MHz
Maximum configuration supported 1s-1s-4s 8d-8d-8d
DMA integration with flash controller YES YES

Optimized OSPI PHY Tuning (valid only for AM263Px)

The OSPI controller on AM263Px SOC integrates a dedicated PHY module which enables flexible and energy efficient transfers. This gives us ability to the flash clock to be used over 50MHz in Single Transfer Rate (STR) mode and 25MHz in Dual Transfer Rate (DTR) mode. This PHY requires software calibration across all the valid values before configuring the PHY_CONFIG_TX_DLL_DELAY_FLD and PHY_CONFIG_RX_DLL_DELAY_FLD in OSPI_PHY_CONFIGURATION_REG. Thus optimizing the software algorithm to span over limited values to complete the calibration in less than 2.5ms.

Refer to AM263Px TRM (13.3.3.6) to learn more about OSPI Controller and PHY module. Application Note on Optimized PHY Tuning here.

Image Format (MCELF)

Multicore ELF, or MCELF is an ELF (Executable and Linkable format) standard based application image format, unlike the previously adopted proprietary RPRC format. An executable file using the ELF file format consists of an ELF header, followed by a program header table or a section header table, or both. The program header table and the section header table's offset in the file are defined in the ELF header. The two tables describe the rest of the particularities of the file. The table summarizes the advantage of MCELF format vs RPRC format.

Table 2 Comparison Between RPRC and MCELF Formats
FeatureRPRCMulticore ELF
Image generation ToolsCustomOpen source
Readable by standard ELF toolsNoYes
Customizable meta dataNoYes
Customizable data segment sizesNoYes
XIPYesYes
Secure boot timeSlowFast

Streaming Support of Secure Boot

Verification of images directly in the flash memory induces a bottleneck due to limited flash clock, and a lack of scratchpad memory leads to Secure Boot images not being able be copied into the memory for the verification. Verification of secure boot images into the external flash also adds a lot of limitations in security by risking the software to TOCTOU attacks. Hence, the streaming secure boot allows users to copy the image into the memory in the SBL and then issuing a call to the TIFS-MCU services to authenticate the image in the streaming mode. This utilizes the execution memory for placement and authentication which in-turn enhances the authentication speed.

Crypto DMA

The DTHE (Data Transform and Hashing Engine) is a wrapper on top of the Crypto IP which is integrated with AM26 device. The DTHE supports EDMA (Enhanced DMA) integration to offload burst data transfers. Enhanced DMA can be programmed to be event-triggered and can automatically transfer the data based on the configured burst size. This allows the Crypto IP events to be configured as EDMA source events allowing complete CPU offload.

Table 3 Crypto Hardware Performance
Data Without DMA (in Mbps) With DMA (in Mbps) Improvement
SHA512
4KB 250.41 679.58 2.7x
16KB 265.65 1024.60 3.85x
AES-CBC-256
4KB 93.61 239.30 2.55x
16KB 94.81 301.54 3.18x

The RSA signature verification are not impacted by the DMA integration in DTHE. For more information, read the PKE hardware integration in TIFS-MCU documentation.

Parallelization of Flash Usage With Secure Boot Services

Next avenue for optimization is in SBL, where the sequential flash reads were modified to do parallel reads. After adding parallelization in SBL to support parallel flash reads of (n+1) th sections while the TIFS-MCU is validating the (n)th sections. Further enhancements were achieved by adding the support for queuing of SIPC messages at HSM server and handling the same in order, for example, the support of sending non-blocking requests and handling of the multiple responses from the HSM on the client (SBL). Below is a visual representation of TIFS-MCU occupied while the SBL is reading from the Flash.

 Boot ParallelizationFigure 1 Boot Parallelization

Secure Boot Benchmark

With the implementation of the previously mentioned techniques, significant increase in the boot time performance is shown and summarized in Table 4.

AM263x

  • SBL size - 55KB. SBL is encrypted as well as authenticated.
  • TIFS-MCU size - 70KB. TIFS-MCU is encrypted as well as authenticated.
Table 4 AM263x Boot Time Performance
Application SizeAuthentication OnlyEncryption + Authentication Only
64KB40.53ms43.40ms
128KB41.05ms44.58ms
256KB45.62ms56.18ms
512KB60.45ms76.39ms
1024KB90.16ms116.92ms
 AM263x Boot PerformanceFigure 2 AM263x Boot Performance

AM263Px

  • SBL size - 60KB. SBL is encrypted as well as authenticated.
  • TIFS-MCU size - 61KB. TIFS-MCU is encrypted as well as authenticated.
Table 5 AM263Px Boot Time Performance
Application SizeAuthentication OnlyEncryption + Authentication Only
1024KB37.11ms64.13ms
512KB32.61ms45.85ms
256KB30.74ms37.48ms
128KB29.83ms33.31ms
64KB29.35ms30.26ms
 AM263Px Boot PerformanceFigure 3 AM263Px Boot Performance

Conclusion

Secure boot has additional run time overhead due to authentication and image integrity verification. However, by employing the software design and hardware offload techniques there is a possibility to improve the secure boot time thus improving the over system performance. In automotive systems, the boot time goals are quite stringent while offering little compromise on the security of the system. The optimized secure boot methods for AM26x family SOC discussed in this paper is targeted to solve the same challenge while utilizing the efficient hardware architecture and software design.

Trademarks

All trademarks are the property of their respective owners.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2024, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale