• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Camera Mirror Systems on AM62A

    • SPRADC4 june   2023 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1

       

  • CONTENTS
  • SEARCH
  • Camera Mirror Systems on AM62A
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2AM62A Processor
  6. 3Vision Pre-processing Accelerator (VPAC)
    1. 3.1 Vision Imaging Sub-System (VISS)
    2. 3.2 Lens Distortion Correction (LDC) Block
    3. 3.3 Multi-Scalar (MSC) Block
  7. 4Deep Learning Acceleration
  8. 5Camera Mirror System Data Flow and Latency
  9. 6End-to-End Functional Safety
  10. 7Example Demonstration
    1. 7.1 Hardware Equipment
    2. 7.2 Software Components
    3. 7.3 Latency Measurement
    4. 7.4 Future Improvement on Latency
  11. 8Summary
  12. 9References
  13. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Technical White Paper

Camera Mirror Systems on AM62A

Abstract

This white paper describes how the AM62A System On Chip (SoC) can be used in automotive-grade camera mirror systems.

Trademarks

Arm® and Cortex® are registered trademarks of Arm Limited.

MIPI® is a registered trademark of Mobil Industry Processor Interface Alliance.

Sony® is a registered trademark of SONY Corporation.

All trademarks are the property of their respective owners.

1 Introduction

Camera mirror systems replace the traditional physical mirrors in vehicles with cameras and displays. A camera mirror system (CMS) uses cameras mounted on the exterior of the vehicle to capture real-time video feeds of the surroundings and display the captured information on displays where traditional mirrors are placed. CMS offers several advantages over traditional mirrors such as providing a wider field of view, reducing blind spots, and enhancing visibility especially in challenging driving conditions. CMS also offers advanced feature capabilities like image enhancement, low light visibility along with the capability of providing pedestrian and vehicle proximity warnings. Recently, the United Nations Economic Commission for Europe (UNECE) established UN regulation no. 151(1), which sets specific requirements and standards concerning the approval of motor vehicles with regards to Blind Spot Information Systems (BSIS) for the detection of bicycles. Next generation CMS systems need to be capable of not only satisfying current and new regulatory standards but also evolve with the quickly changing landscape.

This paper documents how the features in the AM62A processor enable next-generation automotive camera system design. The document also highlights some of the critical considerations when designing a CMS system like latency and functional safety and how the AM62A was designed considering these parameters. AM62A is targeted for 1-1-1 camera systems like a rearview mirror or intelligent side-view mirrors in commercial trucks. The convention 1-1-1 stands for 1 camera, 1 processor, and 1 display. Figure 1-1 shows a typical example configuration. The camera is typically located away from the display unit and for automotive applications FD-Link is typically used for enabling camera data transmission.

GUID-20230607-SS0I-ZDJS-VXNC-VZKLZNTCSB9S-low.svgFigure 1-1 Example Rearview Camera Design With the AM62A

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale