• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AM263x Power Estimation Tool

    • SPRAD54 October   2022 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1

       

  • CONTENTS
  • SEARCH
  • AM263x Power Estimation Tool
  1.   Abstract
  2.   Trademarks
  3. 1Using the Power Estimation Tool
  4. 2Processing Elements
  5. 3Interfaces
  6. 4Power Report
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

AM263x Power Estimation Tool

Abstract

The power estimation spreadsheet provides power consumption estimates based on measured and simulated data; they are provided “as is” and are not ensured within a specified precision. Power consumption depends on electrical parameters, silicon process variations, environmental conditions, and use cases running on the processor during operation. Actual power consumption should be verified in the real system. This tool is meant for estimating power consumption during realistic operating modes; it is not intended for power supply sizing. This power estimation spreadsheet is preliminary and subject to change. This spreadsheet can be downloaded from the web at: https://www.ti.com/lit/zip/SPRR464.

Note: This is a preliminary tool and TI is continuing to characterize more devices; therefore, data is updated and the Power Estimation Tool (PET) revised along with new findings.

Trademarks

All trademarks are the property of their respective owners.

1 Using the Power Estimation Tool

The input part of the spreadsheet consists of following 3 sections: Processing Elements, Interfaces and Power Report.

To use the input part the spreadsheet, users must modify the fields with their appropriate usage parameters. Cells designed for user input are in Yellow. Fields that cannot be modified are Gray. Fields in blue are the output calculated power. Configure the yellow cells to a value most closely aligned with your intended scenario.

The purpose of each of these sections is:

  • Processing Elements:
    • Configure frequency of operation for R5F Dual Core 0, R5F Dual Core 1, HSM M4, ICSSM and CPSW
    • Mode of operation for R5F and HSM (Hardware Security Module)
    • User estimated percent utilization of each core
  • Interfaces
    • Subset of commonly used major Interfaces with selectable mode
    • Subset of commonly used major Interfaces with percent utilization
  • Power Report:
    • Selectable VDD, VDD_SRAM, VDDA
    • Power estimation output by rail
    • Power rails are aligned with AM263x Control card design

2 Processing Elements

This section allows you to set the operating frequency, mode and load each compute core with utilization between 0%-100% (inclusive). Table 2-1 lists the selectable options.

Table 2-1 Selectable Options for Frequency, Mode and Utilization
Processing Element Frequency Mode Utilization
HSM (Hardware Security Module) N/A Secure Boot, Run Time Services 0% – 100%
R5F Dual Core 0 400 MHz, 200 MHz, 0 MHz Dual, Lockstep 0% – 100%
R5F Dual Core 1 400 MHz, 200 MHz, 0 MHz Dual, Lockstep 0% – 100%
ICSSM 200 MHz N/A 0% – 100%
CPSW 200 MHz N/A 0% – 100%

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale