• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AM57xx hardware

    • SPRACK1 January   2019 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL , AM5726 , AM5728 , AM5729 , AM5746 , AM5748 , AM5749

       

  • CONTENTS
  • SEARCH
  • AM57xx hardware
  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
    5.     6
    6.     7
    7.     8
    8.     9
    9.     10
    10.     11
    11.     12
    12.     13
    13.     14
    14.     15
  2. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

AM57xx hardware

AM57xx hardware

The purpose of this guide is to walk hardware designers through the various stages of designing a board on this platform.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

This document follows the structure shown in Figure 1. Each design stage in the Timeline links to a collection of useful documentation, application reports, and design recommendations pertaining to that stage. Using this guide, hardware designers can efficiently locate the resources they need at every step in the board design flow.

hardware_design_timeline_sprabu5.gifFigure 1. Hardware Design Timeline

2 Constructing the Block Diagram

The first step in designing the hardware platform is to create a detailed block diagram. The block diagram should contain all major system ICs and illustrate which I/O ports are used for device interconnection. Below is a collection of resources to aid in the Block Diagram creation process.

  • The links at the TI website below provide block diagrams, application reports, tools, software, design considerations, and other related information for various products under category "Related End Equipments".
    • AM574x Product Folder
    • AM572x Product Folder
    • AM571x Product Folder
    • AM570x Product Folder
  • An EVM (Evaluation Module) is always a good source from which to start building a reference design for these devices. The technical documentation for the EVM is available for download from the following locations:
    • TMDSEVM572X
    • TMDXIDK5728
    • TMDXIDK5718
    • TMDSIDK574
  • The AM57xx family of devices offer a range of performance options while being all designed using the same processing elements and interfaces. This allows that family to be software compatible. Additionally, AM574x, AM572x and AM571x have very similar footprints that allow migration on the same board design. The AM574x/AM572x/AM571x Compatibility Guide covers the differences in ball assignment, pin multiplexing and basic features between AM574x, AM572x, and AM571x.
  • Select from a list of complementary devices to attach to AM57xx device in your system:
    • AM574x Power Management Device (required): TPS659037
    • AM572x Power Management Device (required): TPS659037
    • AM571x Power Management Device (required): TPS659037 or TPS65916
    • AM570x Power Management Device (required): LP87332D + LP873220 or TPS65916

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale