• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Power Line Communication in Solar Applications

    • SNOAAB6 December   2024 AFE030 , AFE031 , AFE032 , OPA2673 , OPA2675 , OPA521 , THS6212 , THS6222 , THS6232 , THVD8000

       

  • CONTENTS
  • SEARCH
  • Power Line Communication in Solar Applications
  1.   1
  2.   2
  3.   Trademarks
  4. IMPORTANT NOTICE
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
Application Brief

Power Line Communication in Solar Applications

Introduction

With the increased number of solar installations, importance of system monitoring and safety rises. In this trend, wired communications play a key role. Safety standards like SunSpec® Rapid Shutdown (RSD) which support NEC 2014, NEC2017 and UL1741 module-level rapid shutdown are built on wired communication interface. Besides the rapid shutdown functionality which is a hard requirement in most installations, module level power electronic (MLPE) monitoring is added to many systems.

Figure 1 shows typical power line communication options implemented in different solar installations. These installations can be divided into communication on DC lines (red) and communication on AC lines (blue). The difference is mainly on how the data-signal is coupled into a power line at a transmitter and how the signal is extracted at the receiver side.

Another option to distinguish is communication from solar panels towards the inverters and the communication towards the grid. Communication between an inverter and MLPE is used for monitoring PV panel operating conditions, fault detection and rapid shutdown. This is applicable for string inverters communicating to power optimizers and other MLPE, or for commercial string or central inverters where string or panel information is collected in combiner-boxes or directly at string input. The second communication option towards the grid is typically used to monitor and control multiple string inverters (done by grid operators to control power levels for grid stability), or in residential use-case to synchronize micro inverters to form split or three phase AC-grid or send operating information from individual micro inverters to a data aggregator.

 Typical Configurations of PLC in Solar InstallationsFigure 1 Typical Configurations of PLC in Solar Installations

Narrowband vs. Broadband PLC

International standards and norms specify the frequency bands which can be used for power line communication. In general, there are two categories, narrowband - and broadband - PLC.

Narrowband PLC uses carrier frequencies up to 500 kHz. Table 1 shows the available frequency bands for different regions. Narrowband PLC has the ability to communicate over wider distances and is often used in Smart Meters. Therefore, narrowband PLC fits very well in Solar to communicate over wider distance from PV-panel to string inverter input.

Table 1 Narrowband PLC Standards and Frequency Bands
RegionOrganizationFrequency Band (kHz)
EuropeCENELEC

3-95

95-125

125-140

140-148.5

JAPANARIB10-450
CHINAEPRI

3-90

3-500

USAFCC10-490

Broadband PLC uses frequencies above 2MHz, thus offering higher data rates and also has lower range compared to narrowband PLC and a significant higher power consumption. A brief comparison is shown in Table 2.

Table 2 Comparison of Narrowband- and Broadband-PLC
Narrowband PLCBroadband PLC
Data rate< 200kbps>1Mbps
Range< 1km< 100m
Frequency bands< 500kHz> 2MHz
Power consumptionLowHigh
ModulationOOK, FSK, OFDMOFDM, QAM, QPSK

Modulation Schemes Used in Narrowband PLC

There are different modulation schemes used in power line communication. In narrowband application On-Off-Keying (OOK), Frequency-Shift-Keying (FSK) and Orthogonal Frequency Division Multiplexing (OFDM) are the most common modulations, while in broadband PLC mainly OFDM is used. In this chapter these three modulation techniques are described in more detail.

On-Off-Keying (OOK)

This simplest form of modulation encodes binary ones and zeros by transmitting a defined carrier frequency for example for a logic “0” or sending nothing for a logic ‘1” (see Figure 2). Both, modulation and demodulation can be done by a simple transceiver like the THVD8000, without the requirement of any additional digital decoding in a microcontroller or processor. To have enough drive capability , when long cables are involved, a line-driver OPAMP like THS6222 or THS6232 in combination with a coupling circuit is needed.

 Power Line Coding Example for OOKFigure 2 Power Line Coding Example for OOK

A reference design that shows how OOK can be used for Solar applications is TIDA-010935. The reference design has all needed circuitry to run a simple OOK modulation. The design is built in a booster-pack configuration that can be controlled by a MSPM0 MCU, but other MCU-booster-packs can be used as well.

Frequency-Shift-Keying (FSK)

In Frequency-Shift-Keying (FSK) different carrier frequencies are used to encode the data in symbols. A symbol is the smalles amount of data which can be transmitted through a communication channel. Depending on the number of frequencies used, a number of bits can be transmitted per symbol. In the simplest form of binary FSK (BFSK) only two frequencies are used. One of the frequencies is used to transmit a logic ‘0’ and the other one is used to transmit a logic ‘1’. In this case those carriers are called mark frequency and space frequency. A variant of BFSK is spread frequency shift keying (S-FSK) which is used in SunSpec RSD. In S-FSK mark and space frequencies are spaced far enough to avoid that narrowband interference disturbs both frequencies. In this way the receiver can still recover data even if one of the two frequencies is blocked by a disturbing signal in the system. Figure 3 shows an illustration of S-FSK.

 Time Domain Coding for S-FSKFigure 3 Time Domain Coding for S-FSK

For demodulation the signal is sampled at least twice the highest carrier frequency. This is typically done by a microcontroller, which also runs the demodulation algorithm. The demodulation algorithm is only sensitive to the specified carrier frequencies, which makes the algorithm robust to broadband noise, but weak against narrowband interference at the exact carrier frequencies. For solar application it is important to keep the switching frequencies of power conversion systems far enough away from the selected carrier frequencies to not impact the communication channel.

TIDA-060001 is a reference design where S-FSK for a SunSpec Rapid Shutdown transmitter or receiver has been realized. The design uses an integrated analog front end IC:AFE031. All needed software for FSK modulation and demodulation is available for TMS320F280049C in the C2000-WARE-SDK, which makes it easy portable to other members of the C2000 Family. For example in the solar-power-optimizer reference design TIDA-010949 the Rapid Shutdown receiver software has been ported over to TMS320F2800137. The reference design works very robust since the power optimizer is running a 300kHz which is far away from the carrier frequencies used in this communication example.

Orthogonal Frequency Division Multiplexing (OFDM)

The last described modulation technique in this article is OFDM. In OFDM, the data stream is divided and transmitted via multiple subcarriers. Orthogonal subcarriers are used to guarantee minimal interference between them. Each subcarrier is modulated with a conventional modulations scheme like phase-shift keying (PSK) or differential phase shift keying (DPSK). Using multiple tightly spaced subcarriers increase the data rate significantly. One example where OFDM is used is in Smart Meters, where standards like G3 and PRIME use OFDM with more than 100 subcarriers. This enables data rates up to a few 100kbit in narrowband operation. OFDM can also be used to increase robustness in noisy environment which is very typical in solar applications. Monitoring the signal quality on the subcarriers and removing those which have a bad signal to noise ratio or using multiple subcarriers redundant increased the overall robustness.

Figure 4 and Figure 5 illustrates an example for OFDM Modulation using four subcarriers. Each of the sub carriers uses PSK to encode one bit. All these signals are summed up and transmitted. The effect of selecting orthogonal subcarriers is shown in the frequency domain. The peaks of the carrier frequencies occur at the zero crossings of the other subcarriers. This provides minimal inter-symbol interference (ISI), in other words increased the robustness of data transmission.

 OFDM Signals in Time DomainFigure 4 OFDM Signals in Time Domain
 OFDM Signals in Frequency DomainFigure 5 OFDM Signals in Frequency Domain

A possible implementation of a PLC transceiver with a C2000 MCU and AFE031 is given in Figure 6. For transmit operation the MCU controls the DAC inside the AFE031 via SPI. The DAC-output is additionally filtered, then amplified and coupled into the power line. For the receive path, the incoming signal is propagating through the line coupling circuit, entering into the programmable gain stage (PGA1), bandpass-filtered again and then being amplified by an additional programmable gain stage (PGA2) before being sampled by the internal ADC of a MCU. All software for encoding and decoding signals is running on the MCU (for example, TMS320F28069 or TMS320F28P550).

 Simplified Line Coupling Circuit for AC MainFigure 6 Simplified Line Coupling Circuit for AC Main

Multiple MCU partitioning are possible as depicted in Figure 7. Running the PLC SW on a dedicated MCU and having a separate MCU for other functions like digital power control. Or combining all into one MCU that runs the power line communication protocol and the digital power control in different interrupt service routines.

 MCU options for power line communicationFigure 7 MCU options for power line communication

Summary

There are different modulation schemes possible for narrowband PLC in solar applications. The pros and cons are summarized in Table 3. For simple low data rate applications OOK can be sufficient. FSK adds some additional robustness and is therefore well suited for safety application with low data rate requirements. In monitoring systems, where a large number of nodes is transferring more data to a data aggregation, the bandwidth of FSK and OOK is not sufficient. In these systems OFDM is a good option.

Table 3 Comparison of Narrowband Modulation Schemes
OOKFSKOFDM
Complexitysimplemoderatecomplex
Data ratelowlowhigh
Robustnesslowmoderaterobust

Trademarks

SunSpec® is a registered trademark of SunSpec Alliance, Inc.

All trademarks are the property of their respective owners.

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale