SNOAA84A January 2022 – February 2022 LM4050QML-SP , LMP7704-SP
Design Goals
Parameter | Value |
---|---|
Common-Mode Voltage (VCM) | 100 V |
Load Current (Iload or Ishunt) | 1 A to 10A |
Output Voltage (Vout) | 0.5 V to 5 V |
Output Voltage Error | < 0.7% |
Power Consumption | < 700 mW |
Total Ionizing Dose (TID) | 100-krad (Si) |
Single Event Latch-up (SEL) Immunity | 85 MeV·cm2/mg |
Design Description
To measure the current in power system health monitoring systems, a shunt resistor is placed either at the high side or the low side of the load. However, placing it at the low side could disturb the load ground. Measuring current at the high side is more preferable in most applications. The following figure shows a high-side current sensing circuit with power supply equal to 100 V and load current varying from 1 A to 10 A. The output of this circuit ranges from 0.5 V to 5 V.
Design Notes
Design Steps
The Op-amp common mode voltage (Vcm) needs to be equal to or greater than the bus voltage (Vbus)
As shown in the previous image, the shunt resistor (Rshunt) and load current (Iload) are used as the inputs for calculating the output percent error. The result shows that the output percent error increases as I_load decreases or R_shunt decreases. Hence, the load current is set to its minimum value (1 A) when picking the R_shunt value to satisfy the minimum requirement in the specification.
In the following curve, to obtain a root sum square (RSS) error less than 0.7%, a 10-mΩ shunt resistor is selected. Even though increasing R_shunt could further increase accuracy, it also increases power dissipation. The part number of the 10-mΩ CSM series shunt resistor selected is Y14870R00100B9W. The resistor has a power rating up to 3 W. With a derating factor of 0.6 (based on EEE-INST-002), the designed shunt resistor power should be less than 1.8 W. With a maximum load current designed to be 10 A, the maximum power consumed by R_shunt is 1 W, which satisfies the requirement.
According to the previous equation, with the 10-mΩ (Rshunt) selected, Vload drops from 100 V to 99.9 V.
With the derating curve found in the shunt resistor data sheet, the self-heating coefficient (θSH) and shunt resistor temperature change (ΔT) are calculated using the following equations.
Plugging the previous equations into the MATLAB tool, the relationship between the load current and temperature change is plotted in the following image. From the curve, the shunt resistor temperature is approximately 33.3°C higher than the surrounding temperature with a full load current of 10 A.
Based on the previous equations, to obtain a Vout range from 0 V to 5 V, with Rshunt equal to 10 mΩ, the ratio of R3 to R6 is calculated to be 50. There are 2 aspects to consider when picking values for R5, R6, and R3:
R6 is set to be 49.9 Ω, and R3 is determined to be 2.49 kΩ for the rest of the calculation. In this application, the Vishay® foil resistor models 303133 to 303138 are selected as a reference for simulation and error calculations. (See the Design References section.)
Parameter | IRF9230 | IRHE9230 | IRHN9250 | IRHNJ597230 |
---|---|---|---|---|
D-S Breakdown [V] | –200 | –200 | –200 | –200 |
Vgs [V] | –2 to –4 | –2 to –4 | –2 to –4 | –2 to –4 |
Zero Gate Voltage Drain Current [μA] | –25 to –250 | –25 to –250 | –25 to –250 | –10 to –25 |
Input Capacitance [pF] | 700 | 1200 | 4200 | 1344 |
Mounting Type | TH | SMT | SMT | SMT |
Size [mm] | 39.37 × 25.53 | 7.94 × 9.41 | 16 × 11.55 | 10.28 × 7.64 |
As shown in the PMOS Comparison table, IRHNJ597230 is selected because it has the smallest IDSS and has relatively small package size and input capacitance.
The shunt reference in the design is to create a virtual voltage supply of 95 V for the LMP7704-SP op amp. The maximum supply current for LMP7704 is 4.5 mA. Hence, the current range of the shunt reference selected must be greater than 4.5 mA.
Shunt Reference Options lists the two shunt reference options for comparison. Both shunt references have a current range greater than 4.5 mA. The reverse breakdown voltage tolerance is not critical in this case, as long as the VEE is around 95 V. Hence, even though the TL1431 has better performance in general, the LM4050QML is preferable because it has a smaller size and requires less components.
Parameter | TL1431-SP | LM4050QML-SP |
---|---|---|
Reverse Breakdown Voltage tolerance (%) | 0.4 | 1.75 |
TID (krad) | 100 | 100 |
Component Needed | 5 | 3 |
Current Range (mA) | 1 to 100 | 0.06 to 15 |
Mounting Type | SMT | SMT |
Size (mm) | 10.16 × 7.11 | 6.86 × 10.41 |
Since the LMP7704 drains a maximum of 4.5 mA, and the shunt reference selected requires at least 0.06 mA, the current through R2 is designed to be 4.75 mA. R2 is calculated with the following formula: