• Menu
  • Product
  • Email
  • PDF
  • Order now
  • DP83848 to DP83826 Hardware Rollover Document

    • SNLA456 April   2024 DP83822H , DP83822HF , DP83822I , DP83822IF , DP83826E , DP83826I , DP83848C , DP83848H , DP83848I , DP83848J , DP83848K , DP83848M , DP83848T , DP83848VYB , DP83848YB

       

  • CONTENTS
  • SEARCH
  • DP83848 to DP83826 Hardware Rollover Document
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Additional Benefits of DP83826
  6. 3Hardware Differences
    1. 3.1 Power Supply and Special Connection Requirements
    2. 3.2 Media Dependent Interface Requirements
    3. 3.3 Hardware Strapping
  7. 4Summary
  8. 5References
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

DP83848 to DP83826 Hardware Rollover Document

Abstract

Texas Instruments offers a variety of Ethernet PHY transceivers which provide designs to multiple end equipment use cases. This application note references the differences between two of the PHYs within the 10/100 Mbps portfolio, DP83848 and DP83826, and how an existing design using DP83848 can be converted to use DP83826.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

Texas Instruments Standard Ethernet PHY portfolio consists of various products. A key differentiator within the portfolio is the datarate each PHY is capable of. There are two classes of groups within the portfolio; 10/100/1000 Mbps PHYs and 10/100 Mbps PHYs. DP83848 and DP83826 are two PHYs within the 10/100Mbps category and share common features aside from data rate such as select MAC interfaces, EtherCAT support, and LED control.

This document is inclusive of all versions of DP83848 and DP83826. DP83848 is available in various temperature rated versions in addition to a second footprint. DP83826 is available in two temperature rated versions and has a ModeSelect pin which, depending on the applied voltage at power-on, can change the PHYs operation and pinout. However for this document, only Enhanced mode is discussed.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale