• Menu
  • Product
  • Email
  • PDF
  • Order now
  • DP83TC811, DP83TG720 Rollover Document

    • SNLA370A December   2020  – December 2020 DP83TG720R-Q1 , DP83TG720S-Q1

       

  • CONTENTS
  • SEARCH
  • DP83TC811, DP83TG720 Rollover Document
  1.   Trademarks
  2. 1Introduction
  3. 2Device Comparison
    1. 2.1 Feature Comparison
    2. 2.2 Pin Map Comparison
    3. 2.3 Strap Comparison
      1. 2.3.1 PHY Address Straps
      2. 2.3.2 MAC Interface, Master/Slave, Autonomous Strap
    4. 2.4 Power-Supply Comparison
    5. 2.5 MDI Comparison
  4. 3Reference Schematics
  5. 4Summary
  6. 5Revision History
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

DP83TC811, DP83TG720 Rollover Document

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

Texas Instruments Automotive Ethernet PHY portfolio consists of 100Base-T1 (DP83TC811) and 1000Base-T1 (DP83TG720) devices. Automotive system qualification cycles are time consuming and any significant change in system can lead to increase in development costs. To reduce the complexity of automotive Ethernet system design, TI PHYs were design such that they can be implemented on a single system. This avoids a complete redesign of the system when going from one speed to the other based on the application requirement. To help achieve this both the devices have the same package footprint of 36 pin QFN, 6mm x 6mm.

Apart from the cable side communication speed,MAC interface selection can also affect PCB design. DP83TC811 supports MII, RMII, RGMII, and SGMII MAC interfaces. DP83TG720 supports RGMII and SGMII MAC interfaces. MII and RMII standards were defined only for 10 and 100Mbps only, so DP83TG720 does not support these options. This application report assumes that DP83TC811 will also be operated in RGMII or SGMII mode.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale