• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Linear Hall-Effect Sensor Array Design

    • SLYA051B October   2020  – May 2024 DRV5055 , DRV5055-Q1 , DRV5057 , DRV5057-Q1 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5273

       

  • CONTENTS
  • SEARCH
  • Linear Hall-Effect Sensor Array Design
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Linear Transit Position Sensing
  6. 3Linear Array Design
  7. 4Absolute Rotational Position
  8. 5Identifying Sources of Error
  9. 6Summary
  10. 7References
  11. 8Revision History
  12. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

Linear Hall-Effect Sensor Array Design

Abstract

Position sensing in mechanical systems using Hall-effect magnetic sensors allows precise control while also providing contact free feedback. This increases overall reliability and durability. Since magnetic fields are able to permeate most materials, the sensor can be placed so that it is protected and isolated from other moving parts of the system. This allows for a great deal of flexibility of design. Hall sensors can be used in detecting angular position, angular rotation speed and direction, proximity, and even absolute position. When moving a magnet along a path, some applications require determination of absolute position. This application note covers how to implement this type of design for long stroke movement where it is necessary to use multiple sensors in a linear array.

Trademarks

E2E™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 Introduction

The best Hall-effect sensor for any given application depends on the type of motion being detected and the various mechanical limitations of the system. Latches and switches operate relative to a fixed threshold. When the sufficient magnetic field is present, the outputs state of these devices changes. Linear sensors however produce a variable output relative to the input magnetic field. Latches and switches are primarily useful where discrete fixed operating positions are used. For example, you might detect the closure of a lid or setting of a 3 position switch using a single DRV5032. Linear Hall-effect sensors are typically needed where absolute position or fine control is required, such as tracking the fluid level in a tank, dial or slider state, or seat adjustment setting.

Selecting a linear Hall-effect sensor depends on system constraints. In the case of long stroke linear transit, the following devices offer design flexibility to suit the application each can provide an appropriate design.

Table 1-1 Comparison of Linear Hall Sensors
DeviceAxis of SensitivityOutput ModePackage OptionsAutomotive Grade Available
DRV5055ZAnalogSOT-23, TO-92✓
DRV5057ZPWMSOT-23, TO-92✓

TMAG5170,
TMAG5170D-Q1

X, Y, ZSPIVSSOP✓
TMAG5173-Q1X,Y,ZI2CSOT-23✓

For simple applications, DRV5055 and DRV5057 can be quickly implemented, and their outputs update immediately upon change in magnetic flux density. However, both of these devices are constrained mechanically due to only having sensitivity along a single axis. TMAG5170 and TMAG5173-Q1 offers three integrated sensors with each sensor oriented along a different axis. This allows the greatest flexibility in system design, and allows the user to observe the entire magnetic flux density. Upon completing each conversion TMAG5170 transmits the resulting digital code over SPI and TMAG5173-Q1 transmits the resulting digital code over I2C, which eliminates the need for an ADC to convert the output signal in both of the device.

In every case, the number of sensors required to implement a linear transit design is primarily dictated by magnet length and the total travel distance. Magnet strength and distance from the sensor also impact the quality of measurement. Fortunately, there is a simple algorithm that scales easily in this application that can be used to determine position of a magnet with an array of sensors.

This discussion demonstrates a basic design procedure focused around DRV5055. The observations and principles discussed apply equally to the DRV5057, TMAG5170 and TMAG5173-Q1. The TMAG5170D-Q1 is a dual-die version of the TMAG5170 that can be used in a system where redundancy is required.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale