• Menu
  • Product
  • Email
  • PDF
  • Order now
  • BOOSTXL-TECDRV BoosterPack™ User's Guide

    • SLVUBX1 December   2020 TPS63810

       

  • CONTENTS
  • SEARCH
  • BOOSTXL-TECDRV BoosterPack™ User's Guide
  1.   Trademarks
  2. 1Introduction
  3. 2Quick Start
    1. 2.1 Step 1: Software Installation
    2. 2.2 Step 2: Firmware Completition and Flashing
    3. 2.3 Step 3: Hardware Setup
    4. 2.4 Step 4: GUI
  4. 3System Overview
  5. 4Hardware Overview
    1. 4.1 Buck-Boost Converter
    2. 4.2 Thermoelectric Cooler (TEC)
    3. 4.3 LaunchPad
    4. 4.4 Voltage Reference
    5. 4.5 Temperature Sensor
  6. 5Firmware Overview
  7. 6Graphical User Interface (GUI)
  8. 7Setup Details
  9. 8Bill of Materials, PCB Layout, and Schematic
    1. 8.1 Bill of Materials
    2. 8.2 PCB Layout
    3. 8.3 Schematic
  10. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

BOOSTXL-TECDRV BoosterPack™ User's Guide

Trademarks

SMBus is a trademark of Texas Instruments Incorporated.

Windows is a registered trademark of Microsoft.

All trademarks are the property of their respective owners.

1 Introduction

The BOOSTXL-TECDRV BoosterPack is an evaluation platform designated to highlight the TPS63810 use as a driver for a thermoelectric cooling (TEC) module.

The BOOSTXL-TECDRV interfaces to LaunchPad development platforms using the XL connector format. To use the BOOSTXL-TECDRV BoosterPack GUI a specific LaunchPad (the MSP-EXP432P401R) must be used. The LaunchPad communicates to the TPS63810 through its I2C interface and also acts as a USB-to-PC GUI communication bridge.

Note:

The BOOSTXL-TECDRV requires a LaunchPad or external master controller to evaluate the TPS63810.

The MSP-EXP432P401R LaunchPad is controlled by commands received from the BOOSTXL-TECDRV BoosterPack GUI. The LaunchPad sends data to the GUI for display. If a LaunchPad is not used, the BoosterPack plug-in module format allows an alternate external host to communicate with the TPS63810 using the LaunchPad connectors.

The BOOSTXL-TECDRV incorporates circuitry and components with the following features:

  • The TPS63810 high efficiency, high output current buck-boost converter with I2C interface.
  • On board precision 2.5-V voltage reference.
  • External power supply and temperature sensors can be connected through screw terminal blocks.
  • I2C interface for the TPS63810 device configuration and communication.

Note:

The BOOSTXL-TECDRV requires an external 3.3-V power supply to power the TPS63810.

Figure 1-1shows the BOOSTXL-TECDRV architecture along with the key components and blocks listed in the features.

GUID-20200909-CA0I-TQQN-Z3PJ-V19PVZGD3BHF-low.gifFigure 1-1 BOOSTXL-TECDRV Block Diagram

2 Quick Start

The quick start presented in this section is a minimalist view of the startup procedure to get the system up and running. More details regarding the hardware and software setup can be found in Section 7.

2.1 Step 1: Software Installation

Download the LaunchPad firmware from the BOOSTXL-TECDRV tools folder . Download and install Energia IDE from the Energia website. The LaunchPad firmware is written in Energia, and needs to be modified for the particular temperature sensor and the TEC module that are used. Alternatively, the Energia code can be used and modified using the cloud CCS tool.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale