• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Using the UCC27624EVM

    • SLUUCE4 June   2021

       

  • CONTENTS
  • SEARCH
  • Using the UCC27624EVM
  1.   Trademarks
  2. 1Introduction
  3. 2Description
    1. 2.1 Features
    2. 2.2 I/O Description
  4. 3Electrical Specifications
  5. 4Test Summary
    1. 4.1 Definitions
    2. 4.2 Equipment
      1. 4.2.1 Power Supply
      2. 4.2.2 Function Generator
      3. 4.2.3 DMM
      4. 4.2.4 Oscilloscope
    3. 4.3 Equipment Setup
      1. 4.3.1 DC Power Supply Settings
      2. 4.3.2 Digital Multi-Meter Settings
      3. 4.3.3 Two-Channel Function Generator Settings
      4. 4.3.4 Oscilloscope Settings
      5. 4.3.5 Bench Setup Diagram
  6. 5Power Up and Power Down Procedure
    1. 5.1 Power Up
    2. 5.2 Power Down
  7. 6Typical Performance Waveforms (CL = 1800 pF)
    1. 6.1 Propagation Delays
  8. 7Schematic
  9. 8Layout Diagrams
  10. 9List of Materials
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

EVM USER'S GUIDE

Using the UCC27624EVM

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The UCC27624EVM is designed to primarily evaluate the UCC27624 performance. The UCC27624 is a 30-V dual channel low-side driver with 5-A peak source and 5-A peak sink current for driving Si/IGBTs/SiC and GaN FETs. The UCC27624EVM board can be used to evaluate other pin-to-pin compatible parts in the supported package. The UCC27624 has low propagation delay and low propagation delay matching between the respective channels rising and falling edges of the driver outputs for reliable timing of the gate-drive signals. The UCC27624 inputs can tolerate signals as high as 26 V regardless of the VDD voltage which enhances device robustness.

The UCC27624 driver includes EN pins which enable the driver's outputs when pulled high, and disables the driver into a low standby current mode when low.

2 Description

The UCC27624EVM is designed to primarily evaluate the UCC27624 functionality. The driver's performances can be evaluated for capacitive loads and/or power devices with provisions for TO-220 footprints. The UCC27624EVM evaluation boards use surface-mount test points allowing connections to INA, INB, ENA, ENB, VDD, OUTA and OUTB UCC27624. For detailed device information, see the UCC27624 DatasheetUCC27624 30-V, 5-A dual channel low-side driver Data Sheet.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale