• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Stacking Implementations with BQ77915

    • SLUA906A January   2020  – September 2020 BQ77915

       

  • CONTENTS
  • SEARCH
  • Stacking Implementations with BQ77915
  1.   Trademarks
  2. 1Configuration
    1. 1.1 General Setup Instructions
  3. 2Functionality
    1. 2.1 Undervoltage (UV)
    2. 2.2 Overvoltage (OV)
  4. 3Troubleshooting FAQ
  5. 4References
  6.   Revision History
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Stacking Implementations with BQ77915

Trademarks

All trademarks are the property of their respective owners.

1 Configuration

The following stacking configuration represents a battery pack protection system for up to 10-S cell pack. Figure 1-1 shows the configuration of the two devices. For configurations with less than 10-S cell pack, only use the two devices. For configurations with 11-S to 15-S cell packs, use three devices. For configurations with 16-S to 20-S cell packs, use four devices.

Note:

For configurations where one or more of the devices supports a lower cell count (for example, three or four) than the rest of the stacked devices, TI recommends using the uppermost device on the stack to support the highest cell count. For example, if the user wants to protect a 9-S cell pack, the top device would support five cells and the bottom device would support four cells. If the user wanted to protect a 17-S cell pack, the top device supports five cells and the lower devices each support four cells. When possible, configure each device to support the same number of cells.

Figure 1-1 Stacking Diagram with HIBERNATE Mode Enabled

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale