• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Introduction to Opto-Emulators

    • SLLA609A September   2023  – October 2025 ISOM8110 , ISOM8610 , ISOM8710 , ISOM8711

       

  • CONTENTS
  • SEARCH
  • Introduction to Opto-Emulators
  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2What are Optocouplers?
  6. 3What is an Opto-Emulator?
  7. 4Classic Circuits Using Opto-Emulators
    1. 4.1 Typical Isolated Power Supply Application Using ISOM811x
    2. 4.2 High-Speed Signal Isolation Using ISOM871x
    3. 4.3 CAN Termination Using ISOM8610
  8. 5Summary
  9. 6References
  10. 7Revision History
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Application Note

Introduction to Opto-Emulators

Abstract

Texas Instruments (TI) opto-emulators combine the behavior of traditional optocouplers with TI’s silicon dioxide (SiO2)-based isolation technology. Despite their preferred isolation performance, digital signal isolators cannot directly replace optocouplers in all circuits due to the analog characteristics of optocoupler inputs and outputs. Opto-emulators bridge this gap by providing equivalent input and output signal behavior while offering pin-to-pin package compatibility with the industry's most popular optocouplers, facilitating seamless integration into existing designs. These products appear just like optocouplers from a system design engineer’s perspective but leverage TI’s expertise for the emulated input and output circuitry and TI's SiO2 isolation barrier technology. Why create such a semiconductor product? The answer is simple: provide designers the best of both worlds.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

Electrical isolation is a means of preventing unwanted direct current (DC) and alternating current (AC) between two parts of a system while still enabling signal and power transfer between those two parts. Signal and power isolation is needed in a wide variety of applications for electrical safety, as well as for the protection of sensitive circuitry under fault conditions, to protect human operators and low-voltage circuitry from high voltages, to improve noise immunity, and to safely withstand ground potential differences between communicating circuits.

Optocouplers, also known as photocouplers, opto-isolators, and optical isolators, are recognized by most design engineers as a common design for achieving galvanic isolation for their system signals. Since optocouplers were one of the first isolators introduced in the semiconductor industry and have been around since the 1970’s, optocouplers have and continue to play a critical role in providing both basic and reinforced safety isolation for most industrial end equipment. While significant improvements have been made to optocoupler technology over the past 50 years, there seems to be a ceiling to their advancement in electrical characteristics, high-voltage reliability, and capability to integrate additional system functionality. This problem has left designers looking for alternative designs to keep up with the pace of their quickly evolving system needs. With semiconductor technological advances in the last couple decades, there are many other isolation technologies, such as capacitive and magnetic isolation, that offer similar functionality as optocouplers with better overall performance. Among the competing technologies is TI’s silicon dioxide (SiO2)-based digital isolation technology. TI has been improving and investing in this technology since the early 2000’s. Before now, this technology has been used to design and grow a vast portfolio of digital isolator products. While digital isolators and optocouplers both provide isolation, (for example, to allow signal communication while blocking high-voltage and breaking ground loops) the two isolator types have plenty of differences that system design engineers must consider.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale