SLAAEB2A December 2023 – August 2025 MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1305 , MSPM0L1306 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The ADC to SPI subsystem example demonstrates how to use the internal ADC to convert an analog signal into a digital representation and transfer the result through SPI. The example configures the MCU to act as an external ADC, receive SPI commands from a SPI controller, and execute the received command accordingly. With simple example commands provided, users can utilize the framework to implement their own commands. Optionally, the MCU can also process the ADC data before transmitting the data through SPI, which is especially useful in applications that need to process the raw data into meaningful values. Download the code for the ADC to SPI example.
The following figure shows a block diagram of the system.
The application requires the internal ADC and 1 instance of the SPI.
Sub-block Functionality | Peripheral Used | Notes |
---|---|---|
Analog signal capture | ADC | Called ADC12_0_INST in code |
Sending ADC data | SPI | Device is the peripheral for this example |
Changes from Revision * (December 2023) to Revision A (August 2025)