• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Low-Power Battery Voltage Measurement Using the On‑Chip VREF and 10‑Bit ADC of MSP430FR4xx and MSP430FR2xx MCUs

    • SLAA828B March   2018  – August 2021 MSP430FR2000 , MSP430FR2032 , MSP430FR2033 , MSP430FR2100 , MSP430FR2110 , MSP430FR2111 , MSP430FR2310 , MSP430FR2311 , MSP430FR2422 , MSP430FR2433 , MSP430FR2512 , MSP430FR2522 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR4131 , MSP430FR4132 , MSP430FR4133

       

  • CONTENTS
  • SEARCH
  • Low-Power Battery Voltage Measurement Using the On‑Chip VREF and 10‑Bit ADC of MSP430FR4xx and MSP430FR2xx MCUs
  1.   Trademarks
  2. 1Introduction
  3. 2ADC Low-Power Sampling Software Design
    1. 2.1 System Clock Source Selection
    2. 2.2 ADC Clock Source Selection
    3. 2.3 Initialization of Unused GPIO Pins
  4. 3ADC Error Correction and Experimental Testing
    1. 3.1 Error Correction
    2. 3.2 Accuracy Test
  5. 4Time-Division Multiplexing of the ADC to Achieve Additional Channel Acquisition
  6. 5Summary
  7. 6References
  8. 7Revision History
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Low-Power Battery Voltage Measurement Using the On‑Chip VREF and 10‑Bit ADC of MSP430FR4xx and MSP430FR2xx MCUs

Trademarks

MSP430 and LaunchPad are trademarks of Texas Instruments Incorporated.

All trademarks are the property of their respective owners.

1 Introduction

The 10-bit ADC module of MSP430FR2xx and MSP430FR4xx products is shown in Figure 1-1. The ADC acquisition channel can directly sample the internal voltage reference (typically 1.5 V, see the data sheet for details), and the ADC reference voltage can be configured as the supply voltage. The ADC input channel detailed information can be found in the "ADC Channel Connections" table in the device data sheet. Configure the ADCINCHx bits in the ADCMCTL0 register as defined in the table to use a 1.5-V reference as the input voltage. The reference voltage for the ADC is configured as 000b for the ADCSREFx bits.

GUID-8BB24593-20CD-46DB-A6EF-22811176CC81-low.gif Figure 1-1 On-Chip Measurement of Battery Voltage Diagram

Equation 1 shows how to calculate the 10-bit ADC conversion results.

Equation 1. GUID-DBC3B7D9-1DB4-48BB-B356-BAAA52F49684-low.gif

where

  • NADC = ADC conversion results
  • Vin = Channel acquisition voltage
  • VR+ = Reference voltage positive
  • VR- = Reference voltage negative

Set Vin to the on-chip 1.5-V reference source, set VR+ to VCC, and set VR- to VSS. Equation 2 shows the formula to calculate the supply voltage.

Equation 2. GUID-981CE8FB-2C43-4BAD-86ED-64016764A9B0-low.gif

Compared with the traditional solutions, on-chip ADC detection solution has the following advantages:

  • Power consumption: the traditional method requires a peripheral voltage divider circuit, while the voltage divider circuit gives the system extra power consumption.
  • Cost: the use of on-chip measurement method can save four resistors and a transistor; in addition, it can save 1 to 2 I/O resources.
  • Volume: there is no peripheral voltage divider circuit that can reduce the size of the PCB for users.

2 ADC Low-Power Sampling Software Design

This document lists the main factors that affect power consumption with the on-chip ADC sample solution in MSP430FR4xx/FR2xx devices with 10-bit ADC. The power consumption results are given with different configurations. This example uses the 1.5-V internal reference voltage. Because the ADC trigger signal does not stop or start the 1.5-V internal reference voltage automatically, software can enable the 1.5-V REF and wait approximately 30 µs before triggering the ADC in the RTC interrupt. Software can also stop the reference in the ADC conversion ready interrupt. The following test is based on this approach. Developers can optionally keep the internal reference enabled all the time at the expense of higher power consumption.

Some MSP430FR4xx and MSP430FR2xx devices have a 12-bit ADC with an internal reference voltage that can be turned on and off automatically during an ADC conversion. Besides this exception, the implementation of battery voltage measurement with these devices is similar to the devices with 10-bit ADC; however, implementation details are outside the scope of this document.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale