• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Amplifier Input Common-Mode and Output-Swing Limitations

    • SBOA508 January   2022 INA818 , INA819 , INA823 , INA849 , OPA2392 , OPA391 , OPA392 , OPA396 , OPA397 , OPA3S328

       

  • CONTENTS
  • SEARCH
  • Amplifier Input Common-Mode and Output-Swing Limitations
  1.   Trademarks
  2. 1Single N-FET or P-FET vs Complimentary N-P-FET Input Stage Limitations
  3. 2Example 1: Output Swing Limitation from VCM in an Op-Amp for Low Side Current Sense
  4. 3Bipolar and CMOS Output Stage Topologies and Output Swing Limitations
  5. 4Example 2: Output Swing Limitations With Instrumentation Amplifiers
  6. 5Summary
  7. 6References
  8. IMPORTANT NOTICE
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
APPLICATION NOTE

Amplifier Input Common-Mode and Output-Swing Limitations

Trademarks

All trademarks are the property of their respective owners.

1 Single N-FET or P-FET vs Complimentary N-P-FET Input Stage Limitations

The common-mode voltage range of an amplifier is the range of usable input voltages allowing for linear operation. Depending on the input stage topology, amplifiers may have common mode input range (VCM) which may be limited relative to one or both supply rails; best case scenario is achieved when input voltage range extends slightly beyond both supply rails (rail-to-rail operation). Limitations in the VCM range come from operating voltages needed to bias the transistors in the input stage, and to ensure operation within a linear range (saturation range for MOSFET or active range for bipolar transistors). We’ll illustrate these limitations for MOSFET amplifier input stages. Figure 1-1 shows a simplified representation of an N-channel MOSFET input stage. The stage consists of a current source (single NMOS, Q3, shown for simplicity), a differential pair with input voltage applied to the gate of each transistor, and an active load PMOS current mirror, Q4 and Q5. The NMOS differential pair has an input common mode voltage limitation with respect to the negative rail, –Vs. Performing Kirchhoff’s voltage walk from –Vs to Vin+, we have:

Equation 1. Vin± (min) = –Vs + Vsat(Q3) + Vgs(Q1,Q2)
Vin± (min) = –Vs + 0.1 V + 0.9 V
Vin± (min) = –Vs + 1 V

Therefore, the N-channel MOSFET VCM range is limited to -Vs by a certain voltage as detailed in Equation 1. Note that we make some important assumptions, namely that Vsat of both NMOS and PMOS transistors are perfectly matched and equal to 0.1V (a typical value). Similarly, we assume that Vgs for both NMOS and PMOS transistors are equal and have a value of 0.9V, a typical value to turn on the transistors. With these assumptions in mind, we can say that this simplified NMOS input stage allows input common mode voltage range operation about 1 V from Vs. Performing Kirchhoff’s walk from the opposite end, +Vs to Vin±, we get:

Equation 2. Vin± (max) = +Vs – Vds(Q5,Q4) – Vds(Q1,Q2) + Vgs(Q1,Q2)
Vin± (max) = +Vs - Vgs(Q4,Q5) – Vsat(Q1,Q2) + Vgs(Q1,Q2)
Vin± (max) = +Vs – 0.9 V - 0.1 V+ 0.9 V
Vin± (max) = +Vs – 0.1 V
Figure 1-1 Simplified Representation of an N-Channel MOSFET Input Stage

Given that Vgs typically exceeds Vds for a MOSFET at the edge saturation (Vsat at a minimum, Vgs at a maximum), the maximum VCM comes within Vsat, or 100 mV, of the positive rail, +Vs.

Conversely, the P-channel MOSFET input stage is limited on the positive side, usually on the order of 1 V from positive rail, +Vs. On the negative side, the common mode voltage range of a P-MOSFET can come within Vsata, or 100 mV from the negative rail,-Vs.

To avoid the limitations of the single differential pair input stage, a complimentary N-channel and P-channel MOSFET (CMOS) input stage design can be used. This design uses two input differential pairs (an N-channel MOSFET pair and a P-channel MOSFET pair), a current steering scheme, and a double-folded cacose summing the two input signals (Figure 1-2). Vset is a voltage source used to control the functionality of the diverting transistor Q8. For common mode voltage below +Vs – Vset, Q8 is off, and the drain current (Id) from Q5 (current source) flows straight through the P-channel differential pair (Q1 and Q2). The double-folded cascode allows the drains of Q1 and Q2 to be biased down to Vsat above – Vs, resulting in VCM swing below the negative rail. This allows the VCM to extend a certain voltage, ΔVP, below the negative rail. Similarly, for common mode voltage above +Vs – Vset Q8 is on, and Id is steered from the P-channel pair to the N-channel pair via the current mirror (Q6 and Q7). The VCM range can therefore exceed the positive rail, +Vs, by a certain voltage, ΔVN. To sum it up, this gives an op-amp with this input stage topology a rail-to-rail VCM range as detailed in Equation 3.

Equation 3. + Vs + ΔVN > VCM > – Vs – ΔVP
Figure 1-2 Simplified Representation of a Complementary N-P-FET Input Stage

Now that we understand the rail-to-rail operation of a complementary input stage, we more elaborately address ΔVN and ΔVP. Looking deeper into the complementary input stage amplifier in Figure 1-2, we can see that the rail-to-rail input performance is dependent on the second stage. Using Kirchhoff’s voltage law from the positive rail down to the input, similar to the one performed previously on Figure 1-1.

Equation 4. Vin± (max) = +Vs – Vsat(Q9,Q10) – Vds(Q3,Q4) + Vgs(Q3,Q4)
Vin± (max) = +Vs – 0.1 V – 0.1 V + 0.9 V
Vin± (max) = +Vs + 0.7 V

We can see from Equation 4 above that the complimentary input stage amplifier has input common mode range 0.7 V above the positive rail. We can find the common mode input voltage range to the negative rail by performing the same procedure.

Equation 5. Vin± (min) = – Vs + Vsat(Q11,Q12) + Vsat(Q1,Q2) – Vgs(Q1,Q2)
Vin± (min) = – Vs + 0.1 V + 0.1 V – 0.9 V
Vin± (min) = – Vs – 0.7 V

From Equation 4 and Equation 5 we find that the common mode input voltage range extends beyond the positive and negative rail typically by about 0.7 V, which is represented by the aforementioned terms ΔVN and ΔVP. In data sheets, you will notice that most rail-to-rail amplifiers are specified up to 0.1 V (not 0.7 V) beyond the supplies. This is due to the protection diodes between the input and each rail.

2 Example 1: Output Swing Limitation from VCM in an Op-Amp for Low Side Current Sense

As an example, let’s assume that we are working with OPA391 operational amplifier, which we have in a gain of 100 V/V, powered with a 5.0-V single supply. Let's say we want to measure current between 0 and 50 A, and we choose a 1-mΩ shunt resistor. This means we will see differential input in the range of 0 to 50 A × 1 mΩ = 50 mV. The minimum VCM value for OPA391 is 0.1V below ground, so our input conditions are in agreement with the data sheet requirements. However, OPA391 AOL output conditions are specified in the range of –Vs + 0.1 V < Vout < +Vs – 0.1 V. Therefore, between 0 and 0.1 V and 4.9 V to 5 V of output the op-amp may encounter some non-linearity, which is undesirable. We can solve the issue quite easily:

  • We can level-shift the input common mode up by 1 mV (which is amplified by the closed loop gain), or level shift -Vs down by 100 mV. Level shifting the input can be achieved through a simple voltage divider circuit, or providing headroom for the output can be accomplished by providing a small negative rail. If no negative rail is present in the system, a negative charge pump like the LM7705 solves that problem in a single IC. In either case, it will put Vout at least 100 mV above –Vs under 0 current condition, which resolves the output swing issue on the low end. Take note that either solution also exceeds the maximum linear operating range on the high end, which is in violation of the output voltage swing specifications. We can solve that issue by decreasing the gain of the circuit or the value of the shunt resistor slightly to bring Vout (max) at or below +Vs – 100 mV.

While the complementary input stage described offers an excellent solution to the input common mode problem, it is important to keep in mind that the transition between each pair will generate a change in the input offset voltage of the amplifier, also known as input crossover distortion. The transition can be eliminated by keeping both pairs conducting at all times, but this is often avoided because of the excessive power dissipation required. The input crossover distortion can be circumvented more elegantly by using a zero-crossover amplifier (Zero-crossover Amplifiers: Features and Benefits tech note). These amplifiers use a single transistor pair and an integrated charge pump to push the internal voltage supply enough beyond the nominal value to remain in linear operation.

3 Bipolar and CMOS Output Stage Topologies and Output Swing Limitations

The output swing range of an amplifier is the range of output voltages allowing for linear amplifier operation. As with VCM, the output swing (Vout) limitations are related to operating voltages of transistors in the output stage. Depending on the application and topology, Vout may be more or less limited relative to the rails, regardless whether they are single, dual, or asymmetric. Perfect rail-to-rail performance does not exist in practice, although some of the complimentary MOSFET designs come fairly close.

Many applications require Vout swing to only one rail, typically the negative rail. The earliest op-amp output stages accomplished this by having an NPN emitter-follower configuration with a resistive pull-down (Figure 3-1 A). A pull-down resistor to the negative rail allows the output to approach the negative rail, but this greatly limits the sinking current and results in slow output response. A similar design (bipolar or MOSFET) utilized NPN/NMOS current sources in place of the pull-down resistor, offering higher gain and near to-negative-rail output swing (Figure 3-1 B).

With the advent of modern complimentary bipolar processes, better matched, high speed PNP and NPN transistors became available. As a result, the complimentary emitter-follower output stage (Figure 3-1 C) was developed with its most significant advantage being low output impedance. The major drawback of this topology is its limited output swing, typically on the order of 1V or more to the rail due to transistor operating voltages in the stage. Specifically, the minimal forward-bias voltage across the PNP current source (VFB-P), and the base-emitter voltage (VBE-N) limit swing to positive rail, whereas the VFB-N of the NPN current source and the VBE-P limit swing to negative rail. Full output voltage swing of the complimentary bipolar output stage is thus:

Equation 6. +Vs - Vsat (npn) - Vbe (pnp) > Vout > -Vs + Vsat (pnp) + Vbe (npn)

More recent complimentary common-emitter or common-source output stages (Figure 3-1 D and Figure 3-1 E), allow the op-amp output swing much closer to rail, but both of these stages have fairly high output impedance. For the bipolar version of this stage, the output swing limitation to each rail comes from Vce, (sat), or the minimal collector-emitter voltage needed to keep each transistor operating in the linear region. The typical Vsat for a bipolar transistor is 300mV at 25ºC and changes by roughly -2mV per each ºC increase in temperature.

Equation 7. -Vs + Vsat < Vout < +Vs - Vsat

We can perform a similar analysis to the MOSFET version of this stage, illustrated in Figure 3-1 (E). The output swing limitation comes from the MOSFET on-resistance (Ron) while in the triode region, which causes an output voltage range limitation relative to the rail equal to Id × Ron. In essence, in the non-linear operating region, the MOSFET acts as a small resistor and produces a voltage drop. Under unloaded conditions, Id = Iq, the limitation caused by the voltage drop is on the order of 5 mV to 50mV, which is considered almost truly rail-to rail performance.

Equation 8. -Vs + Id x Ron > Vout > +Vs + Id x Ron

Keep in mind, that under normal operation Id is equal to the quiescent current of the output transistors, Iq, plus the load current. In other words, the output swing will decrease as the load current increases. A plot illustrating this effect is included in data sheets – look for the output voltage swing vs output current plot (often known as a claw curve). Operate within the range of the curves to remain in linear operation

Figure 3-1 Common Output Stage Topologies

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale