SBAA545 August 2022 DRV5013 , DRV5013-Q1 , TMAG5110 , TMAG5110-Q1 , TMAG5111 , TMAG5111-Q1
Auto body motor modules enable many of the luxuries found in modern automobiles. Motor modules consists of a gear train and an electric motor, usually packaged in a shared housing, and are used to drive a geared lever or pulley system that in turn moves a mechanical accessory, like a window, car seat, or sun-roof. This application note uses a window regulator to illustrate the interaction between the mechanical assemblies of the regulator and their impact on the magnet and Hall-effect sensors used to monitor the motor in the regulator.
E2E™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.