• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Comparing ADS114S06 and ADS114S08 to the Lower-Cost ADS114S06B and ADS114S08B

    • SBAA287B May   2018  – December 2022 ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B

       

  • CONTENTS
  • SEARCH
  • Comparing ADS114S06 and ADS114S08 to the Lower-Cost ADS114S06B and ADS114S08B
  1.   Understanding the Differences Between the ADS114S06 and ADS114S08 Standard and Cost-Optimized Versions
  2.   Trademarks
  3. 1Introduction
  4. 2Performance
  5. 3Features
  6. 4Specifications
  7. 5EVM Differences
  8. 6Alternative Device Recommendations
  9. 7Conclusion
  10. 8Revision History
  11. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Comparing ADS114S06 and ADS114S08 to the Lower-Cost ADS114S06B and ADS114S08B

1 Understanding the Differences Between the ADS114S06 and ADS114S08 Standard and Cost-Optimized Versions

This document describes the differences between the standard and cost-optimized versions of the ADS114S06 and ADS114S08 (ADS114S0x) devices. Texas Instruments provides cost-optimized, B-grade versions of each device for systems that may not require the performance level and feature set offered by the standard devices. Table 1-1 lists the standard versus B-grade devices.

This application note also describes how the differences apply to the ADS114S08 evaluation module (EVM) because there is no dedicated EVM for the B-grade versions.

Table 1-1 Standard Versus B-Grade Devices
Standard Device B-Grade Device
ADS114S06 ADS114S06B
ADS114S08 ADS114S08B

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The 6-channel ADS114S06 and 12-channel ADS114S08 are 16-bit, 4000 sample-per-second (SPS), delta-sigma analog-to-digital converters (ADCs). These devices offer an integrated analog front-end that consists of:

  • A fully-flexible input multiplexer
  • Dual excitation current sources (IDACs)
  • A low-noise programmable gain amplifier (PGA)
  • A low-drift 2.5-V voltage reference with buffered reference output
  • A temperature sensor
  • A precision oscillator
  • Multiple monitoring and diagnostic features

The ADC performance and feature set make these devices an excellent choice for all types of precision sensor measurements in end-equipment such as:

  • Pressure transmitters
  • Temperature controllers
  • Temperature transmitters
  • PLC analog input modules

Figure 1-1 illustrates the functional block diagram for these two ADCs.

GUID-CE3C278F-4770-4069-B851-149E40B19EED-low.gifFigure 1-1 Functional Block Diagram

The differences between the standard and B-grade versions are separated into three different categories:

  • Performance
  • Features
  • Specifications

These categories are discussed in detail in the following sections.

2 Performance

The ADS114S06B and ADS114S08B have some relaxed specifications to help optimize cost and enable use in end-equipment that does not require the performance of the standard-grade ADCs. Table 2-1 summarizes these relaxed specifications and compares their values to the standard-grade devices.

Table 2-1 Performance Differences Between the ADS114S0x and ADS114S0xB
PARAMETERTEST CONDITIONSADS114S06
ADS114S08
ADS114S06B
ADS114S08B
UNIT
MINTYPMAXMINTYPMAX
Operating ambient temperature–50125–40125°C
Absolute input currentPGA enabled, all gains0.1±20.1±10nA
INL (best fit)PGA bypassed,
VCM = AVDD / 2
1101ppmFSR
PGA enabled, gain = 1 to 8, VCM = AVDD / 2215225
PGA enabled, gain = 16 to 128, VCM = AVDD / 2315225
Gain errorTA = 25°C, PGA bypassed0.004%0.012%0.01%0.1%
TA = 25°C, PGA enabled,
gain = 1 to 32
0.004%0.012%0.025%0.2%
TA = 25°C, PGA enabled,
gain = 64 and 128
0.004%0.02%0.025%0.2%
VREF accuracyTA = 25°C, TQFP package–0.05%±0.01%0.05%–0.2%±0.01%0.2%
TA = 25°C, QFN package–0.1%±0.01%0.1%–0.2%±0.01%0.2%
VREF temperature driftTA = –40°C to +85°C2.58840ppm/°C
TA = –50°C to +125°C310N/A
IDAC accuracy (each IDAC)TA = 25°C, 10 µA to 100 µA–5%±0.7%5%–6%±1%6%
TA = 25°C, 250 µA to 2 mA–3%±0.5%3%–6%±1%6%
IDAC current mismatchTA = 25°C, 10 µA to 100 µA0.15%0.8%0.20%
TA = 25°C, 250 µA to 750 µA0.1%0.6%0.20%
TA = 25°C, 1 mA to 2 mA0.07%0.4%0.20%
IDAC temperature drift10 µA to 750 µA20120100ppm/°C
1 mA to 2 mA1080100
IDAC temperature drift matching10 µA to 100 µA32510ppm/°C
250 µA to 2 mA21510
Oscillator accuracy–1.5%1.5%–2%2%
Device costADS114S06ADS114S06BUSD ($)
ADS114S08ADS114S08B

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale