• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Integrating Dynamic Ground Projection Into a Vehicle

    • DLPY012 June   2022 DLP2021-Q1 , DLP3021-Q1

       

  • CONTENTS
  • SEARCH
  • Integrating Dynamic Ground Projection Into a Vehicle
  1.   At a glance
  2.   Authors
  3.   What is DGP and what can DGP be used for?
  4.   What are the different electronics architecture options for DGP? What are the tradeoffs of each architecture?
  5.   How can I get started evaluating DGP?
  6. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

MARKETING WHITE PAPER

Integrating Dynamic Ground Projection Into a Vehicle

This paper highlights how DLP technology can support different use cases for dynamic ground projection and the architectures needed to support them.

At a glance

1 What is DGP and what can DGP be used for?
Dynamic Ground Projection is a new feature that small dynamic projectors can enable all around the car.
2 What are the different electronics architecture options for DGP? What are the tradeoffs of each architecture?
Different electronics architectures can support multiple use cases for the modules. OEMs can design the projector to enable different levels of flexibility and feature support.
3 How can I get started evaluating DGP?
Texas Instruments has a number of tools to help you get started developing a dynamic ground projection solution today.

Authors

Brandon Seiser
Product Marketing Engineer
DLP Automotive

What is DGP and what can DGP be used for?

For a long time, small exterior lights only had the capability to illuminate the area around the car and were not used to customization or personal features. In the past few years, we have seen an increase in the functionality of these lights with the ability to display single color patterns. Using Texas Instruments DLP® technology, these lights can be transformed into fully dynamic projectors when designed with devices such as the DLP3021-Q1 and DLP2021-Q1. DLP technology is automotive qualified, compact and reprogrammable, enabling a system that can display an infinite number of full color images and videos for vehicle personalization, customization and styling. This application is called dynamic ground projection, as lighting designers finally have a dynamic projection system to display information all the outside of the car.

A projector system about the size of a human thumb can be easily integrated into many areas around the call, such as side rearview mirrors, door panels, rocker panels and tail lights. When mounted in these locations, dynamic ground projection systems can be used to create animated logos, customizable welcome messages, unique light carpets for vehicle styling, and extended displays for turn signals and advanced warnings. While our dynamic ground projections systems can act as standalone modules, connecting them to the vehicle’s communication network enable a truly dynamic display that the can further connect a driver to their car.

What are the different electronics architecture options for DGP? What are the tradeoffs of each architecture?

What makes the DLP3021-Q1 and DLP2021-Q1 products different from the rest of Texas Instruments’ DMDs, is their ability to display content without a graphics processing unit (GPU). These DMDs can be display content that has been pre-processed and stored in flash memory. An FPGA in the system retrieves the content from memory and loads the bit planes to the DMD. By removing the need for a video bus and GPU, dynamic ground projection systems can be easily integrated anywhere in the vehicle. The DGP system can be connect to the vehicle’s CAN-FD or Ethernet network to enable updates to the flash memory or reloading new content and images to the projection module.

Our dynamic ground projection architectures support three distinct user experience options following a good, better, best offering model. First, there is a solution that enables an exterior small light replacement. The exterior small light replacement is the entry solution for dynamic ground projection as this is the easiest option to integrate, but comes with the lowest content flexibility. Second, there is a solution to enable user content selection and delayed content updates. This option enables the vehicle to update the flash memory, but does not enable the streaming of live video data. Finally, there is a solution to enable live video streaming from a GPU for the highest system performance and flexibility. Each of these architectures services a unique purpose which allows OEMs and Tier 1s to create a portfolio of dynamic ground projection offerings for different vehicle trim levels.

Our exterior small light replacement architecture is the simplest and most cost-effective solution. This solution inspired the DLP3021LEQ1EVM and DLP2021LEQ1EVM electronics designs and is meant to serve as a replacement to existing small lights. The only input signals required for modules with this architecture are power rails and this solution displays content almost instantaneously after power is supplied. While this solution is ideal for someone looking to replace a puddle light, the flash memory in the system cannot be updated without the module being removed from the car. If dynamic ground projection is only desired for vehicle styling, this architecture is the most cost-effective way to enable dynamic projections. Figure 1 highlights how DLP technology can generate images, without being connected to the vehicle’s ECU. The module position is shown by the green dots, and the ECU is highlight in yellow at the front of the car. While this image shows the DGP modules mounted in the doors, these modules can be mounted anywhere in the car as long as power rails are accessible. Both the DLP3021-Q1 and DLP2021-Q1 DMDs can support this architecture.

GUID-20220609-SS0I-K89T-TCLB-PSGN6C2TJTMR-low.jpg Figure 1 Exterior small light replacement architecture requirements.

The architecture required to enable user selected content is a bit more complicated than our exterior small light replacement, as the modules need to be connected to the vehicle’s central ECU. The easiest way to enable this experience, is to connect the ECU to the modules with CAN-FD or Ethernet. These connections enable new data to be sent to the module and store in flash memory. A SPI command can be sent to the module to enable different images or videos to be played on demand from the user or vehicle’s automated driver assistance system (ADAS). The user may be able to select various welcome or leaving scenarios, and receive updates for specific holidays based on the vehicle’s location. Additionally, if the DGP module is used during operation of the vehicle, the DGP modules can communicate with surrounding pedestrians to project the intent of the vehicle and extend turn signals. With a more complex system, vehicle manufacturers can enable a brand-new experience each time a user approaches the vehicle. Figure 2 shows the DGP modules’ connection to the central ECU. This system design restricts mounting locations to areas that can connect back to the ECU. The blue highlighted paths depict and example routing of the CAN-FD or Ethernet connections for the DGP modules. Both the DLP3021-Q1 and DLP2021-Q1 DMDs can support this architecture.

GUID-20220609-SS0I-GTNZ-CBHK-9JGBSVDPFKR0-low.jpg Figure 2 Vehicle infrastructure routing to connect the DGP module to the central ECU.

While the previously discussed architectures focused on cost-conscious implementation of DGP and integration into existing vehicle networks, the highest performance architecture uses live video streaming to display content. Live video streaming can be accomplished by routing a video bus from the central ECU to the DGP module in a similar fashion to the aforementioned architecture. An example of how a video bus could be routed is shown below in Figure 3. Routing a video bus comes with its own challenges, but results in the most dynamic system, as the desired content can be generated on the fly and immediately displayed by the DGP module. Content for customization, styling, branding in addition to ADAS information can be displayed, turning the area around the vehicle into a display. This architecture is only supported by the DLP3021-Q1 DMD with the DLPC120-Q1 DMD controller, which replaces the FPGA used in the exterior small light and user content selection architectures.

GUID-20220609-SS0I-VKNC-GFSF-8787QX83N97P-low.jpg Figure 3 Live video streaming routed to DGP modules in the vehicle's taillights.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale