DLPA083B june 2019 – april 2023 DLP2000 , DLP2010 , DLP230KP , DLP230NP , DLP3010 , DLP3030-Q1 , DLP3310 , DLP4620S-Q1 , DLP4710 , DLP471TP , DLP500YX , DLP5500 , DLP5530-Q1 , DLP5530S-Q1 , DLP5531-Q1 , DLP5533A-Q1 , DLP6500FLQ , DLP6500FYE , DLP650LNIR , DLP670S , DLP7000 , DLP7000UV , DLP9000 , DLP9000X , DLP9000XUV , DLP9500 , DLP9500UV
The purpose of this document is to summarize the optical properties that are most important in estimating the efficiency of a Digital Micromirror Device (DMD) in a projection system.
All trademarks are the property of their respective owners.
The next three sections discuss the fill factor, window optical properties, and the active mirror array properties, respectively. This report concludes with a discussion on calculating the overall efficiency.
As discussed in more detail in Section 6, overall optical efficiency can be
estimated using
Equation 1.
where
Overall DMD efficiency is generally a product of fill factor, window transmission, diffraction efficiency, and mirror reflectivity, which are described in more detail in the following sections.