• Menu
  • Product
  • Email
  • PDF
  • Order now
  • SimpleLink™ Wi-Fi® CC3100, CC3200 Radio Tool

    • SWRU556 June   2021 CC3100 , CC3200

       

  • CONTENTS
  • SEARCH
  • SimpleLink™ Wi-Fi® CC3100, CC3200 Radio Tool
  1.   Trademarks
  2. 1 Introduction
  3. 2 Features
  4. 3 Prerequisites
    1. 3.1 Software Downloads
    2. 3.2 Hardware
  5. 4 Radio Tool Installation Directory
  6. 5 Hardware Connections
    1. 5.1 CC31xxBOOST Plus CC31XXEMUBOOST
      1. 5.1.1 Using the UART Interface
      2. 5.1.2 Using the SPI Interface
    2. 5.2 CC32xx-LAUNCHXL
  7. 6 Flashing the Board
  8. 7 Running the RadioTool GUI
    1. 7.1 Set Up Tab and General Information
    2. 7.2 GUI TX Testing
    3. 7.3 GUI RX Testing
  9. 8 Current Measurement
  10. 9 CLI Version
  11. 10Insertion Loss Calibration
  12. 11Hardware Connections on Non-TI EVMs
  13. 12Source Code for Developers
    1. 12.1 RadioTool Application Sources
    2. 12.2 CC32xx Application Source
  14. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

USER'S GUIDE

SimpleLink™ Wi-Fi® CC3100, CC3200 Radio Tool

Trademarks

SimpleLink, Texas Instruments, BoosterPack, LaunchPad, Code Composer Studio are trademarks of Texas Instruments Incorporated.

Wi-Fi are registered trademarks of Wi-Fi Alliance.

Bluetooth is a registered trademark of Bluetooth SIG, Inc.

Microsoft is a registered trademark of Microsoft Corporation.

All trademarks are the property of their respective owners.

1 Introduction

The SimpleLink™ MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With an ultimate goal of 100 percent code reuse across host MCUs, Wi-Fi®, Bluetooth® low energy, Sub-1 GHz devices, and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit (SDK) lets you reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.

The main use of the Radio Tool is to serve as a control panel for direct access to the radio. The tool can be used for the radio frequency (RF) evaluation, and for certification purposes (such as FCC, ETSI, Telec, and so on). The tool is expected to work seamlessly on TI evaluation platforms: BoosterPack plus FTDI emulation board for CC31xx devices, and LaunchPad for CC32xx devices. If customers want to use the tool on their final platform, see Section 11. The I/O levels of these lines should be kept at VBAT level (the same voltage that powers the CC31xx and CC32xx devices).

For reference RF numbers, see the CC3120 SimpleLink™ Wi-Fi® Wireless Network Processor, Internet-of-Things Solution for MCU Applications Data Sheet and the CC3220 SimpleLink™ Wi-Fi® Wireless and Internet-of-Things Solution, a Single-Chip Wireless MCU Data Sheet.

2 Features

  • Connection
    • CC3120/CC3135 through the serial peripheral interface (SPI)
    • CC3120/CC3135 through the universal asynchronous receiver/transmitter (UART)
    • CC3220/CC3235x through the UART
  • Acquires MAC address
  • Acquires firmware information
  • TX – Transmission testing
    • Continuous
    • Packetized
    • Carrier Wave (CW)
  • RX – Receiver testing
    • Statistics
    • Rate histogram
    • RSSI histogram

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale