• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Dual-Mode Bluetooth®CC2564C Evaluation Board

    • SWRU495C March   2020  – December 2021 CC2564C

       

  • CONTENTS
  • SEARCH
  • Dual-Mode Bluetooth®CC2564C Evaluation Board
  1.   Trademarks
  2. 1Introduction
  3. 2 CC256XCQFN-EM Kit Contents
  4. 3 CC256XCQFN-EM Requirements
  5. 4 CC256XCQFN-EM Board Overview
  6. 5 CC256XCQFN-EM Board Settings
    1. 5.1 EM Connector Settings
    2. 5.2 COM Connector Settings
  7. 6Revision History
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

QUICK START GUIDE

Dual-Mode Bluetooth®CC2564C Evaluation Board

Trademarks

MSP432 and LaunchPad are trademarks of Texas Instruments.

Bluetooth is a registered trademark of Bluetooth SIG, Inc.

All trademarks are the property of their respective owners.

1 Introduction

The TI CC256XCQFN-EM board is used to evaluate the dual-mode Bluetooth CC2564C controller, which supports classic Bluetooth and Bluetooth low energy (LE) wireless technology. The CC256XCQFN-EM board works with the following hardware development kits:

  • MSP-EXP432P401R with BOOST-CCEMADAPTER (through EM connectors)
  • TMDXEVM3358 AM335x Evaluation Module (through COM connector)
  • CC256XEM-STADAPT with STM32 MCU Evaluation Board (through EM connectors)
Note:

Refer to the CC256XEM-STADAPT Quick Start Guide for a list of compatible STM32 MCU Evaluation Boards.

The CC256xC Bluetooth device is a complete basic rate (BR), enhanced data rate (EDR), and LE host controller interface (HCI) solution that reduces design effort and enables fast time to market. Based on TI’s seventh-generation core, the module is a product-proven solution supporting Bluetooth 4.2 dual-mode protocols (5.1 compliant).

Figure 1-1 shows the CC256XCQFN-EM board.

GUID-75C0744A-EBF8-4DCB-B298-550AFFDAF382-low.png Figure 1-1 CC256XCQFN-EM Board

2 CC256XCQFN-EM Kit Contents

The CC256XCQFN-EM kit contains the following contents:

  • One CC256XCQFN-EM board with a TI dual-mode BluetoothCC2564C controller

3 CC256XCQFN-EM Requirements

For a complete evaluation, the CC256XCQFN-EM board requires hardware and software tools selected from the following lists.

  • Hardware requirements:
    • MSP432™LaunchPad™ (sold separately), AM335x Evaluation Module (sold separately), or other MCU platforms (sold separately)
      • MSP432 LaunchPad board options:
        • MSP-EXP432P401R
        • BOOST-CCEMADAPTER
        • CC3200AUDBOOST (optional: only necessary for audio and voice applications like A3DP, HFP, and HSP)
        Note: The BOOST-CCEMADAPTER and CC3200AUDBOOST pinout are not compatible with each other. Because of this limitation, the CC3200AUDBOOST cannot be stacked on top of the MSP-EXP432P401R and BOOST-CCEMADAPTER. Refer to the CC2564C TI Dual-Mode Bluetooth Stack on MSP432 MCUsUser's Guide for the CC3200AUDBOOST pin connections for audio and voice applications.
      • AM335x Evaluation Module options:
        • TMDXEVM3358
      • Other MCU options:
        • CC256XEM-STADAPT
        • STM3240G-EVAL or one of the STM32 MCU platforms mentioned in the CC256XEM-STADAPT User’s Guide.
  • Software requirements:
    • TI dual-mode Bluetooth stack
      • On MSP432 MCUs: CC2564CMSP432BTBLESW
      • Other MCUs: CC2564CSTBTBLESW
      • On Sitara Processors (Linux): TI-BT-4-2-STACK-LINUX-ADDON

Figure 3-1 shows example hardware setups for the CC256XCQFN-EM board using the MSP-EXP432P401R LaunchPad and the BOOST-CCEMADAPTER boards.

GUID-54B21538-02E2-4E63-A505-8D0FAF57EBC9-low.png Figure 3-1 MSP432™ LaunchPad™ Hardware Setup Example

Figure 3-2 shows the example hardware setup for the CC256XCQFN-EM board using the CC256XEM-STADAPT and the STM3240G-EVAL board.

GUID-17ECCAEB-5552-4A2B-A2FF-D7D39C9E8C95-low.png Figure 3-2 STM3240G-EVAL Hardware Setup Example

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale