• Menu
  • Product
  • Email
  • PDF
  • Order now
  • SimpleLink WLAN Access Point

    • SWRA654A December   2019  – April 2020 CC2652R , CC2652R7 , CC2652RSIP

       

  • CONTENTS
  • SEARCH
  • SimpleLink WLAN Access Point
  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
      1.      6
      2.      7
      3.      8
      4.      9
        1.       10
        2.       11
        3.       12
      5.      13
    5.     14
  2.   15
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

SimpleLink WLAN Access Point

SimpleLink WLAN Access Point

This application report presents the benefits and the possibilities in extending an existing WLAN Access Point to use an additional IoT protocol such as Zigbee®, Thread, or Bluetooth® Low Energy. It will present the different technologies and what they can be used for. It will also present the proposed hardware solutions and example applications.

Trademarks

Code Composer Studio is a registered trademark of Texas Instruments.

Bluetooth is a registered trademark of Bluetooth SIG, Inc.

Wi-Fi is a registered trademark of Wi-Fi Alliance.

Zigbee is a registered trademark of ZigBee Alliance.

All other trademarks are the property of their respective owners.

1 Introduction

Why settle for a Wi-Fi™-only WLAN Access Point when you can create a smart access point? Adding Bluetooth Low Energy, Zigbee, or Thread to the access point will enable the use of localization, provisioning, and IoT for smart building. The TI coexistence feature will allow multiple protocols to operate at the same frequency, coexist, and not transfer data simultaneously. When two RF protocols are used in the same MCU, the Dynamic Multi-protocol Manager (DMM) is used to allow the protocols to operate concurrently. This will innovate enterprise, retail, and medical environments.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale