• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Acoustic Noise in Home Appliances Due to Torque Ripple in Motor Drives – Part 2

    • SSZTBL1 february   2016

       

  • CONTENTS
  • SEARCH
  • Acoustic Noise in Home Appliances Due to Torque Ripple in Motor Drives – Part 2
  1.   1
  2.   2
    1.     3
    2.     Cogging Torque in BLDC Motors and PMSMs
    3.     Effects of Torque Ripple
    4.     Conclusion
    5.     Additional Resources
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
Acoustic Noise in Home Appliances Due to Torque Ripple in Motor Drives – Part 2

Seetharaman Devendran

Manu Balakrishnan

In part 1 of this series, I reviewed various factors that cause torque ripple in brushless motors, including torque ripple caused by commutation and DC-bus voltage ripple. In part 2, I’ll look at “cogging torque,” which is another source of torque ripple in brushless motors.

Cogging Torque in BLDC Motors and PMSMs

Cogging torque in brushless direct current (BLDC) motors and permanent magnet synchronous motors (PMSMs) is caused by motor design aspects: the interaction between the permanent magnets (PMs) of the rotor and the stator slots. It is also known as detent or “no-current” torque. Many low-cost, simply constructed BLDC motors have higher cogging torque. In such motors, the cogging torque can be felt by manually turning the rotor shaft at a low speed. The rotor will align in a number of stable positions even when the machine is unexcited, resulting in a pulsating torque. This torque is position-dependent and its periodicity per revolution depends on the number of magnetic poles and stator slots. Because cogging torque can cause torque ripples and induce vibrations (particularly at light loads and low speeds), its reduction is usually a major design goal.

You can reduce the amplitude of cogging torque by selecting a proper slots/pole ratio during machine design. You can also substantially reduce cogging-torque amplitude with motor-design approaches such as reducing the slot opening, shaping the magnet pole, skewing the magnet or slot, or increasing the air-gap length. All of these efforts will come at the expense of added complexity in motor construction and some loss of output torque, however.

At very low speeds, high cogging torque can cause relatively large speed fluctuations, even causing the motor to stop or move in discrete increments. Cogging torque reduction is very important for low-velocity applications like robotics and servo. In servo control, precise positioning is impossible with a traditional proportional-integral controller due to the nonlinearity of cogging-torque ripple. When a motor spins at high speeds, cogging torque ripple creates high-frequency speed fluctuations that generate acoustic noise and vibration.

Figure 1 shows a typical cogging-torque waveform of a 24-slot 4-pole PMSM with a rated torque of 15-N m.

GUID-9F94EB41-A37B-4991-BB43-444D5DC400BC-low.jpg Figure 1 Cogging torque of a four-pole PMSM

Because most low-cogging-torque motors come with added cost due to machine design complexity, an alternative approach to minimize the effect of cogging-torque ripple amplitude is through drive control design using a compensation term in the control scheme.

Although several methods are available for the compensation of cogging torque, a common method used in servo drives is to initially put the system into “learn mode” to create a look-up table of cogging torque at various rotor angles for a full revolution. From the look-up values, applying a counteracting waveform with the correct frequency and phase relation to the actual cogging torque will result in amplitude reduction of the cogging torque.

Effects of Torque Ripple

Torque ripple-induced vibration in fans and blowers can become even more amplified because of other mechanical system components, creating acoustic noise. The effects of torque ripple are undesirable in some demanding motion control and machine-tool applications because they can lead to speed oscillations that deteriorate performance. In addition, torque ripple may excite resonances in the mechanical portion of the drive system producing the acoustic noise, and in machine-tool applications, leave visible patterns in high-precision machined surfaces. I recommend analyzing cogging torque for the application of high-precision position control, especially at low speeds.

Conclusion

Effect of torque ripple on acoustics and overall performance is discussed in this two part series. This knowledge can help in the selection of motors such as BLDC or PMSM, and semiconductor components such as sinusoidal motor controller or high performance microcontroller for FOC implementation and high bandwidth amplifiers for current sensing.

Additional Resources

  • Check out these reference designs:
    • TI Designs 230-V, 250-W, High Efficiency BLDC Motor Drive w/DC Bus Voltage Ripple Compensation Reference Design.
    • Mains Operated, 24V, 30W BLDC Motor Drive w/Highly Efficient, High Power Factor Power Supply.
    • Read these IEEE articles: Torque ripple minimization in direct drive systems and Torque Ripple Reduction of BLDC Motors by Modifying the Non-Commutating Phase Voltage.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale