• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Digitally Select Your Reference Voltage

    • SSZTBD7 august   2016 LM4041-N , TLV431

       

  • CONTENTS
  • SEARCH
  • Digitally Select Your Reference Voltage
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
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
Digitally Select Your Reference Voltage

Christopher Dean

Adjustable voltage references offer great flexibility to circuit designers because the reference is not limited to the manufacturer’s pre-set values. The adjustable output is typically configured with a voltage divider from the output to the feedback pin, as shown in Figure 1. To regulate the output, compare the voltage at the feedback pin to an internal reference (shown in this post as VREF_INT), typically 1.2V. The device adjusts the output until VFB and VREF_INT match.

Some adjustable shunt references such as the LM4041 maintain VFB across R1; some maintain VFB across R2, such as the TLV431. I’ll concentrate on the LM4041, but the concepts apply equally to other adjustable shunt references by switching R1 and R2 in the equations. In this blog post, I’ll describe one possible method of changing the resistor divider and in turn changing the reference voltage with digital signals.

GUID-9FE95DDC-2189-4DFC-9FD0-165C4DE078A1-low.png Figure 1 Typical vREF Feedback Divider

The method involves replacing the two fixed resistors with a single digital potentiometer. Figure 2 demonstrates this conceptually, where the feedback pin is connected to the wiper of the potentiometer and the high and low side are connected to VREF and GND, respectively.

GUID-DED81F30-2B70-40C7-BB92-0AC2A2CD70AE-low.png Figure 2 Potentiometer Center Tap (Wiper) Connected to Feedback

Figure 3 shows the circuit redrawn, with the TPL0102 digital potentiometer acting as the voltage divider. You can configure a digital potentiometer to act as a voltage divider by connecting a voltage across the high and low pins of the internal resistor and connecting the output to the wiper pin. The wiper position affects the ratio of the resistance between the wiper and the high and low pins, and its position is controlled digitally by sending a code word to the device. The TPL0102 uses an I2C interface, while other potentiometers are available with serial peripheral interface (SPI) or parallel interfaces.

GUID-2F355981-05DC-430B-B32A-1DA512D28B9A-low.png Figure 3 VREF With the TPL0102 Digital Potentiometer as the Feedback Divider

Because the ratio of the resistances sets the output voltage, the absolute values of the divider resistors are not critical. This allows you to easily replace the resistor divider with a digital potentiometer. Equation Figure 1 illustrates the relationship between the adjusted output, VREF_OUT and the resistance ratio:

GUID-4F7383AD-8A37-462F-81E5-3C48E722AA9F-low.png Figure 4 (1)

That is an important point in this application, as the absolute resistance value of digital potentiometers can vary quite a bit, while the ratio of the resistances is very accurate. For example, to generate a 3.3V reference voltage, the required resistance ratio of R2-to-R1 is 1.66.

The potentiometer data sheet provides the formulas to calculate the output of the voltage divider for a given code, shown in Equations 2 and 3. VHW is the voltage from the high pin (H) to the wiper (W), while VWL is the voltage from the wiper (W) to the low pin (L):

GUID-4783B56A-87B9-4DD6-B2DE-6623CE64CE4B-low.png

VFB is across R1, as I mentioned in the introduction, so let’s continue with Equation 2, which calculates the voltage between the high pin and the wiper pin. The wiper is connected to the feedback pin of the device, and VFB is forced to VREF_INT. Equation Figure 1 shows the formula solved for the digital code required for VREF_OUT:

GUID-6F140DC6-F263-442D-A386-741EEF4C8041-low.png Figure 5 (4)

Continuing the example in Equation Figure 1 where NTAPS is 256, VREF_INT is 1.24V and V­REF_OUT is 3.3V, you’ll need to write decimal code 160, which yields resistance values for R1 and R­2 of 37.50kΩ and 62.50kΩ, respectively. More importantly, the ratio of these two resistances is 1.66, also calculated using Equation Figure 1:

GUID-D6CFC9AC-914B-4165-BD34-73DB644459FC-low.png Figure 6 (5)

If you need to change the reference voltage, you simply need to write an I2C transaction to move the wiper position accordingly. As a result, the voltage at the feedback pin changes and adjusts VREF_OUT. You can also use the potentiometer to digitally tune the reference voltage, where the greater the number of taps in the potentiometer, the finer the resolution in the resistance ratio and therefore the finer the resolution in the output reference voltage.

A limitation of using a digital potentiometer in this application is the voltage limit of the digital potentiometer integrated circuit (IC), which typically cannot exceed 5.5V. Confirm that the resistance ratio does not get set to a condition that would present a VREF_OUT greater than 5.5V. For a 256-tap digital potentiometer and a shunt reference with an internal reference of 1.24V, the decimal code should not exceed 200. Figure 7 demonstrates the effect of the input code on the reference voltage for a 256-tap potentiometer and a 1.24V-referenced device.

GUID-B1DDF4C1-1179-4904-B871-D98B3C892A42-low.png Figure 7 Reference Voltage vs. Digital Potentiometer Code

Enable and configure the potentiometer before powering the shunt reference to ensure that the resistor divider is correctly in place. If that is not possible, you can add a large resistance in parallel with the resistor that is not acting as the drop for VFB. That would be 1MΩ from the feedback pin to ground (across R2) for the LM4041, or 1MΩ from the feedback pin to the output (across R­1) for the TLV431.

To avoid an extra parallel resistance, you can configure the device with fixed R1 and R2 resistors and a digital potentiometer in series with one of them. You would then have to configure the potentiometer as a rheostat, shown in Figure 8. This configuration depends on the absolute resistance of the digital potentiometer, which is not as accurate as when using it as a ratiometric voltage divider, and requires feedback to the microcontroller for final digital-code selection.

GUID-34DD488C-DC0C-409C-8799-5C06E2714208-low.png Figure 8 Fixed Resistors with Digital Potentiometer as a Rheostat

Now that you understand how an adjustable voltage reference sets it output voltage, you know how to use this to your advantage to change the output voltage dynamically.  If the application already uses a microcontroller, including a digital potentiometer can add some versatility to a seemingly simple part.

Additional Resources

  • Learn more about TI’s voltage reference products.
  • Download the white paper, “Voltage Reference Selection Basics,” for a detailed explanation of voltage-reference selection with respect to analog-to-digital converter (ADC) resolution.
  • Read the Open Systems article, “Shunt vs. series: How to select a voltage reference topology.”
  • Read TI’s blog series, “Understanding Voltage References,” which discusses the applications of both shunt and series references and when to use them.
  • Start your design in WEBENCH® Power Designer.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale