• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Small Doesn’t Mean You Compromise Performance When Implementing Signal Isolation

    • SSZTA59 may   2017 ISOW7841

       

  • CONTENTS
  • SEARCH
  • Small Doesn’t Mean You Compromise Performance When Implementing Signal Isolation
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Small Doesn’t Mean You Compromise Performance When Implementing Signal Isolation

Neel Seshan

A couple of years ago, when I was working with interfaces in the industrial market, the size of the device package was never a showstopper. Fast-forward a few years, and device package size is sometimes a deciding factor as to whether you can use it in your application.

Industrial application functionality is increasing while size is decreasing, similar to the consumer market, but on a smaller scale. The challenge is now with semiconductor manufacturers to provide smaller package solutions without losing performance. This is true in the isolator space as well; but with isolators, there are certain dimension requirements for high-voltage creepage and clearance demands. But still smaller is better.

In my last post, I discussed the ISOW7841, which integrates isolated data and power in a single package and can replace the discrete solution (dotted section) shown in Figure 1.

GUID-9A6B4889-0BFF-43F3-BC9D-BF7A47841069-low.jpg Figure 1 Isolated Data and Power Subsystem

This integrated solution is smaller than the discrete solution which incorporates a transformer driver, transformer, rectifier and regulator (as shown in Figure 2).

GUID-906826F7-AE7B-4CA2-AB9F-E62FFAC36581-low.png Figure 2 Size Comparison of Discrete and Integrated Isolated Data and Power Subsystem Board Layouts

On the left side of Figure 2, you can see the board layout with the discrete components needed to build an isolated data and power solution.  On the right side, the design is simplified by just one component with two decoupling capacitors. The size of the design drops from 35 mm-by-28 mm to 22 mm-by-15 mm, around 33% of the discrete solution’s board space.

But is that the only savings you can expect from a single-chip solution? No. Here are some additional benefits:

  • Board height. An external transformer can be bulky and often much thicker than small-outline integrated circuit (SOIC) packages. As Figure 3 shows, the discrete solution uses a 4.10-mm thick isolation transformer. The integrated solution with planar transformers in a 16-pin SOIC package (shown in Figure 4) has a thickness of 2.65 mm, which is about 35% smaller in height compared to the discrete transformer. When you want to stack multiple boards in space-constrained applications, the smaller height of the integrated solution will come in handy.
GUID-6BA47339-564B-4D34-998A-EA0B9DFBD35F-low.jpg Figure 3 Discrete Solution for Isolated Power with a 4.10mm-thick Isolation Transformer
GUID-D7BB3B05-D322-4126-BE6C-351C0B770CD1-low.png Figure 4 ISOW7841 Evaluation Module with Planar Transformers in a 2.65mm-thick 16-Pin SOIC Package
  • Certifications. Almost all designers get their systems certified by agencies such as Underwriters Laboratories (UL), Verband der Elektrotechnik (VDE), etc. These certifications require that components on the board meet the prescribed standards. Having a discrete solution not only adds to the number of components requiring certification, but it may also delay the process if any of the certified components are unavailable. For example, it may be difficult to find a transformer with the right certifications, especially with reinforced ratings. An integrated chip simplifies this process because the isolated signal and power solution is certified as a single unit. Every TI isolator is certified by agencies like UL, VDE, Canadian Standards Association (CSA) and TÜV SÜD. Most certifications are available within six months of device release.
  • Simplicity. Systems involving an isolated power supply need protection from overloading and short circuits. For instance, a malfunction of the circuit and possibly increased device temperatures will occur if the voltage drops due to the load and the current continues to rise. Having overload-protection features like thermal shutdown and current limiting will prevent damage to the device and circuit.

Another feature that is nice to have in isolated power supplies is the soft-start mechanism, which ensures controlled in-rush current and avoids any overshoot on the output during power up. Figure 5 compares the VCC and output voltage VISO waveforms of the ISOW7841 with a similar device on the market. Any overshoot at the output could potentially damage the load circuits. The soft-start scheme in the ISOW7841 limits primary peak currents drawn from the VCC supply and charges the VISO output in a controlled manner, avoiding overshoots.

These features (thermal shutdown, current limiting, soft-start) in the ISOW7841 device reduce the amount of external protection circuitry in the design, thereby simplifying it.

GUID-89BBA24D-33F4-47AB-B02A-629D84AFEFB4-low.png Figure 5 VISO Power-up Oscilloscope Capture Compares VISO Waveforms of the ISOW7841 with a Similar Device on the Market

The next time you are looking for space-saving isolation devices, look at more than the device’s XY dimensions. Additional device benefits may make your design smaller and your time to market faster.

Additional Resources

  • Check out the ISOW7841 data sheet.
  • Watch the video, “Reinforced Isolation and Power: An Integration Story.”
  • Download the white paper, “Fully integrated signal and power isolation – applications and benefits.”
  • Learn more about designing with low emissions in the article, “How to achieve low radiated emissions with fully integrated data and power isolation.”

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale