• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Making Industrial Communication Easy with AMIC110 SoCs

    • SSZTA46 June   2017 AMIC110 , DP83822I

       

  • CONTENTS
  • SEARCH
  • Making Industrial Communication Easy with AMIC110 SoCs
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Making Industrial Communication Easy with AMIC110 SoCs

Bryan Trinh

Industrial Ethernet protocols are an important part of factory automation. Today, there are many protocol standards including EtherCAT, Profinet, Powerlink, Ethernet/Industrial Protocol (IP) and Sercos III. Having so many different protocols makes it challenging to develop solutions that can work for several different networks. One solution is to have a single device that’s reprogrammable for different protocols, like TI’s newly announced AMIC110 system on chip (SoC).

TI Sitara™ ARM® processors can enable more than 10 industrial communication standards through the programmable real-time unit industrial communications subsystem (PRU-ICSS). Adding a full-featured ARM® processor may be impractical if there is already an existing applications processor on the design. If that’s the case, you can leverage your existing work but also enable PRU-ICSS functionality by adding a communications processor like the AMIC110 SoC. Although the AMIC110SoC contains an ARM Cortex®-A8 core, it serves to run Ethernet stacks instead of acting as the primary processor.

As a communication processor, the AMIC110 SoC provides a flexible alternative over static solutions. One advantage is that the AMIC110 SoC’s software programmability makes it possible for you to run different communication standards instead of being tied to just one. That makes it possible to reuse the same device in different projects that use different protocols. The re-programmability also makes it easier to upgrade if a protocol releases a feature change, or completely reprogram the SoC in case a new protocol is released. These qualities make the AMIC110 SoC an excellent way to add industrial communication to a device.

For example, a motor-control application may use a C2000™ microcontroller (MCU) to control a motor, as shown in Figure 1. To add a protocol like EtherCAT, the C2000 MCU can communicate to the AMIC110 through Serial Peripheral Interface (SPI), and the AMIC110 SoC will handle the protocol-based communication to the rest of the network.

GUID-827138C7-E340-4116-BE5E-8283FCE1B5E0-low.jpg Figure 1 Example Implementation of Motor Control with AMIC110 and C2000

AMIC110 SoCs are part of the Sitara processor family and share many of its benefits, like using the processor software development kit (SDK) as a standard software platform. The processor SDK makes it easy to migrate software between Sitara processors, which reduces learning time on new processors and enables you to leverage existing work well into the future.

Additional Resources

  • Learn more about the DP83822I industrial Ethernet PHY.
  • Start developing with the AMIC Industrial Communications Engine (ICE).
  • Add industrial communications to your C2000 project with the EtherCAT Slave and Multi-Protocol Industrial Ethernet Reference Design.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale