• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Visualizing the Performance of the Low-energy Accelerator

    • SSZT930 october   2017 MSP430FR5994

       

  • CONTENTS
  • SEARCH
  • Visualizing the Performance of the Low-energy Accelerator
  1.   1
  2.   2
    1.     3
    2.     4
    3.     Additional Resources
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
Visualizing the Performance of the Low-energy Accelerator

Caleb Overbay

Today’s electronics engineers are constantly challenged with the need for high performance while maintaining low power. The balance between these two seemingly conflicting ideas is at the heart of every design and is crucial to success in today’s market. Consider a gas-metering application, for example. These devices are often located in remote areas and require long battery life, high accuracy and high reliability.

The Ultrasonic Gas Meter Front End with MSP430™ Reference Design makes efficient use of the low-energy accelerator (LEA) available on the MSP430FR5994. During implementation of this reference design, the LEA demonstrated the performance and power consumption improvement outlined in Table 1.

Table 1 Processing and Power Consumption with and without the LEA
Parameter Using LEA Not using LEA
GASMETERING_runAlgorithm() execution time 12.8ms 93.7ms
Current consumption attributed to algorithm over one sample per second (MCLK = 8MHz) 19.78µA 144µA

You can now visualize these benefits with the help of the LEA graphical user interface (GUI), created using GUI Composer and the MSP430FR5994 LaunchPad™ development kit. This GUI quickly compares the execution of complex vector math operations using the central processing unit (CPU) and the LEA module. LEA GUID shows the basic layout of this new tool and how the bar graphs make quickly comparing LEA processing with the traditional CPU method simple and easy.

GUID-D48B3995-C0A2-4713-A0AF-FFA174C59E6B-low.png Figure 1 LEA GUID

The website https://dev.ti.com/gallery offers access to a wide range of GUI Composer demonstrations including the LEA GUI. This GUI also takes advantage of a powerful energy-based code analysis tool called EnergyTrace™ software that’s built into various MSP430 devices. This technology enables you to measure and display an applications energy profile. In this GUI, it’s used to measure the average power consumed by the MSP430FR5994 while it continuously runs a function using the CPU or LEA peripheral.

Here’s how the demo works:

  • When you first open it, instructions will appear to guide you through the GUI.
  • Select the MSP430 device via the drop-down menu and click the CONNECT button.
  • The GUI will program the device if you’ve checked the Auto Program checkbox, or you can manually program the device with the PROGRAM DEVICE button.
  • Select the function you want to test, along with the length and the order.
  • Once you click the Play button, the MSP430 MCU runs the function multiple times using the LEA and measures the average power and cycles. The demo then runs the same function multiple times using the CPU.
  • A bar graph displays the data for both, where you can see the drastic improvement that the LEA offers.

The LEA GUI shows the true benefit of using the LEA module for vector-based processing such as fast Fourier transforms (FFTs), finite impulse filters (FIRs) and infinite impulse response (IIR) filters. You can quickly see the difference it can bring to your applications.

You don’t have to take my word for it either. Visit the TI store and pick up a MSP430FR5994 MCU LaunchPad development kit (MSP-EXP430FR5994) to test the LEA GUI yourself.

Additional Resources

  • Download the white paper, “Setting a new standard for MCU performance while minimizing energy consumption.”
  • Learn more about smart gas-metering solutions.
  • Discover more about the performance and advanced signal processing that the LEA can provide in the application report, “Benchmarking the Signal Processing Capabilities of the Low-Energy Accelerator on MSP430 MCUs.”

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale