• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Accurate Frost or Ice Detection Based on Capacitive Sensing

    • SSZT777 march   2018 FDC2214

       

  • CONTENTS
  • SEARCH
  • Accurate Frost or Ice Detection Based on Capacitive Sensing
  1.   1
  2.   2
    1.     3
    2.     Current Solutions
    3.     Frost or Ice Detection Based on Capacitive Sensing
    4.     Test Results
    5.     Sensor Placement Recommendations
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Accurate Frost or Ice Detection Based on Capacitive Sensing

Richard Wang

The accumulation of frost or ice on an evaporator coil always presents a challenge in home appliances such as refrigerators, freezers and air conditioners. The accumulation of frost or ice insulates the air circulating through the evaporator unit, which makes maintaining the overall temperature difficult. Also, atmospheric conditions that lead to the formation of ice block the heat exchange: the thicker the frost, the worse the efficiency. Figure 1 shows an efficiency comparison with different frost thicknesses based on one model of refrigerator.

GUID-B97A4313-4C1D-4F5D-A053-311B250DBF50-low.png Figure 1 Comparison by Cooling Down a Fixed Amount of Water

Current Solutions

Solving these problems requires a defrosting system that is operatively associated with the heat exchanger. The question is when to activate the defrost cycle. One easily implemented method is to include a clock, which at some pre-selected interval shuts the compressor off and turns on a thermal heating device adjacent to the evaporator coils, melting the frost or ice. Another popular method uses temperature-sensitive devices such as a negative temperature coefficient (NTC) thermistor to measure the temperature of the refrigerating medium as one parameter. The disadvantage of these methods is that frost or ice does not always accumulate at a constant rate, depending on the ambient humidity and air temperature. Defrosting on a regular time cycle, whether necessary or not, is inefficient and wastes electrical power.

The most effective method is to directly sense the quantification of frost and ice buildup on the cooling body and initiate countermeasures at the proper time. A controller, operatively coupled to a frost detection sensor (or sensors) and to the defrosting system, selectively activates the defrost system to initiate a defrost cycle of the evaporator in response to a signal that indicates the presence of frost formation on heat-exchange tubes and heat-transfer fins.

Frost or Ice Detection Based on Capacitive Sensing

Capacitive sensing enables a more reliable solution for measuring the thickness of frost or ice. The Texas Instruments (TI) Capacitive Frost or Ice Detection Reference Design, Resolution of <1mm, Temperature Drive <0.25% detects the amount of frost and ice accumulated on the surface of a cooling body using capacitive-sensing technology. The capacitance of a sensor changes according to the thickness of frost or ice because of the variation of the dielectric constant between air and frost or ice. Let me explain the basic principles.

Capacitance is the ability of a capacitor to store an electrical charge. For a parallel plate capacitor, Equation 1 calculates the capacitance as:

Equation 1. C=Q/V

where C is the capacitance related by the stored charge, Q, at a given voltage, V.

The capacitance (measured in farads) of a parallel plate capacitor (see Figure 2) consists of two conductor plates and is calculated using Equation 2:

Equation 2. C=εr×ε0×Ad

where A is the area of the two plates (in meters), is the dielectric constant of the material between the plates, is the permittivity of free space (8.85 × 10-12 F/m) and d is the separation between the plates (in meters).

GUID-AC003CE2-3DA8-45B9-80FD-27AC0DE57EA5-low.gif Figure 2 Parallel Plate Capacitor

Capacitive sensing is a technology based on capacitive coupling. A basic capacitive sensor is anything that is metal or a conductor and detects anything that is conductive or has a dielectric constant different from the air. Capacitance can be detected to sense different applications by changing one of the parameters while keeping the rest constant. Table 1 shows the dielectric constant of some materials.

Table 1 Material Dielectric Constants
Material Dielectic Constant (Ɛᵣ) Comment
Air 1 -
Water 80 at 20°C
Glass 7.6 to 8.0 -
Paper 2.3 -
Ice 3.2 -

The accumulation of frost and ice on the surface of a cooling body causes the capacitance between two parallel plates (the metal surface of the cooling body and a specifically designed sensor) to change due to the equivalent dielectric constant change, as shown in Figure 3. When a properly designed sensor composed of a conducted material is fixed on the surface of a cooling body, the parameters for d, and A remain constant. The capacitance will be a function of the equivalence of, which is the basic principle of frost and ice detection.

GUID-212D0FE0-F12D-4A29-BD7A-92B2E20B9019-low.svg Figure 3 Model for Frost and Ice Detection Based on Capacitance

Table 1 shows that the dielectric constant of ice is three times greater than that of air and the dielectric constant of water is up to 80 times greater. When ice or water is positioned between the parallel plate capacitor, the capacitance increases with the thickness.

Figure 4 shows an example of the expected capacitance change curve based on a copper mesh sensor. In Stage 1, the capacitance remains a constant value when there is no frost or ice on the dry surface of a cooling body. At the beginning of Stage 2, the refrigerator or air-conditioner compressor starts to work and frost or ice accumulates on the surface of the cooling body. Due to the dielectric constant change from air to ice (see Table 1), the capacitance increases based on the thickness of the frost or ice. The defrost cycle activates when the desired thickness has been detected. The capacitance experiences a sharp change when ice (= 3.2) turns to water (= 80), shown in Stage 3, and then returns back to the original value after the water drops from the cooling body.

GUID-4493E76D-54F5-4DAF-9CCC-6C6922D6E057-low.jpg Figure 4 Capacitance Change in Principle

Test Results

I built a test platform based on a refrigerator. Figure 5 shows the frost formation process on the surface of the evaporator, and Figure 6 shows the capacitance-change curve during one cycle. The six pictures labeled in Figure 5 correspond to the six points, also labeled, in the curve of Figure 6. This system uses capacitance values to calculate the amount of frost.

GUID-6637D5C5-8D9A-4A8B-A71D-A6ADA7FB50C2-low.gif Figure 5 Frost Formation Process
GUID-848EC930-CC66-4780-8FAA-95C2C5F8697E-low.png Figure 6 Sensed Capacitance During the Frost Formation Process

To measure the capacitance, I used TI’s FDC2214, which is a high-resolution capacitive-to-digital converter. The devices employ an innovative narrow-band based architecture to offer high rejection of noise and interferers while providing high resolution at high speed. The test results verify that this is a robust and cost effective solution which could solve the problem of frost or ice detection in refrigeration system and significantly improve the system efficiency. Using relative values rather than absolute values of capacitance is a good way to improve the system reliability even under complex environmental conditions.

Sensor Placement Recommendations

Two options are proposed for the placement of sensors.

Option 1: The sensor can be two plates made by any conductive material (e.g. Aluminum foil shown in Figure 7). The two plates are placed on both side of evaporator and the capacitance is measured between these two plates.

GUID-0CE22C42-CF52-41A2-9ECB-BED1D1D14D58-low.png Figure 7 Two Plate Sensor Model

The conductive plates are recommended to integrate inside the plastic housing of evaporator, which is shown in Figure 8.

GUID-AFC8B4C7-BDDA-43A0-AE93-6453F89511E1-low.png Figure 8 Two Plate Sensor Installation

As is shown in Figure 8, the two conductive plates are recommended to place inside the plastic housing (one in front and one in back) of evaporator so that air flow will not be affected.

Option 2 (Preferred): Take the evaporator as one plate of sensors. In this option shown in Figure 9, only one external conductive plate is needed which lowers cost. Due to safety consideration and ESD protection in some cases, an external safety capacitor (e.g. Y capacitor, 1nF) is added in series with the sensor instead of in parallel.

GUID-0201807C-DC90-450B-AE98-1350A4F3F053-low.png Figure 9 Single Plate Sensor Model

In the instance when only one plate is used, it is easy to integrate inside the plastic housing of evaporator, which is shown in figure 10. The air gap between the evaporator and sensing plate depends on the required defrost thickness and is often times around 4mm-10mm.

GUID-096CDF16-30A4-49C7-A5D1-44B594805CFB-low.png Figure 10 Single Plate Sensor Installation

Additional resources

  • Find the best solutions for your next-generation appliance designs.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale