• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Configure Your MSP430 MCU's Analog Signal Chain Using the Smart Analog Combo GUI

    • SSZT660 July   2018 MSP430FR2355

       

  • CONTENTS
  • SEARCH
  • Configure Your MSP430 MCU's Analog Signal Chain Using the Smart Analog Combo GUI
  1.   1
  2.   2
    1.     3
    2.     What Is a Smart Analog Combo?
    3.     The MSP-EXP430FR2355 LaunchPad™ Development Kit
    4.     How to Get Started with the Smart Analog Combo GUI
    5.     What You Can Do with the Smart Analog Combo GUI
    6.     Generating a Signal Using the Internal 12-Bit DAC
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
Configure Your MSP430 MCU's Analog Signal Chain Using the Smart Analog Combo GUI

Christopher Vendette

Imagine a world where you can easily configure your analog options on the fly without any need to change onboard components.

The Smart Analog Combo module integrated within the MSP430FR2355 MCU that allows you to do just that. The MSP430R2355 MCU contains four of these modules, giving you the tools and flexibility to realize your design.

What Is a Smart Analog Combo?

As you can see in Figure 1, the Smart Analog Combo module is an integrated configurable analog block that is configurable as an operational amplifier (op amp), programmable gain amplifier (PGA) or 12-bit digital-to-analog converter (DAC) without having to change any external hardware components.

GUID-093629D7-168D-4F74-80FD-B82C141BE8A4-low.png Figure 1 Smart analog combo module diagram

The module’s easy configurability enables you to save time; its integration within the MSP430™ MCU opens up board space; and the fact that you can configure the module through software allows for maximum future-proofing flexibility.

The Smart Analog Combo, combined with the 105°C maximum operating temperature rating of the MSP430FR2355, enables this MCU to provide a robust option for projects such as smoke detectors/fire safety devices, battery packs and much more.

The MSP-EXP430FR2355 LaunchPad™ Development Kit

The MSP-EXP430FR2355 LaunchPad development kit in Figure 2 is the evaluation tool for the MSP430FR2355.

GUID-8DB4DBE6-B08C-4E7F-A489-27383FB8C4DD-low.png Figure 2 MSP-EXP430FR2355 LaunchPad development kit

The Smart Analog Combo graphical user interface (GUI), as seen in Figure 3, is a demo for the MSP-EXP430FR2355 LaunchPad development kit enables you to evaluate the power of the integrated configurable analog on the MSP430FR2355 MCU with an interface full of sliders, drop-down selections and visual representations. In the demo, you can generate a function using the DAC, measure your own signal using the pins of the LaunchPad™ development kit, or measure the output with the on-chip 12-bit analog-to-digital converter (ADC).

GUID-F59D305A-746A-43EF-936E-07B959E9C60C-low.png Figure 3 Smart Analog Combo GUI

How to Get Started with the Smart Analog Combo GUI

Plug in your MSP-EXP430FR2355 LaunchPad development kit using the included Micro-USB cable. Go to dev.ti.com on your web browser. Your device should be auto-detected, as noted on the left. Select Run Interactive Demos from the GUI Composer Gallery, or go to dev.ti.com/gallery and search for “MSP-EXP430FR2355,” as shown in Figure 4. Select the out-of-the-box demo from the options.

GUID-23F031C3-9D36-4A52-A1F7-5A8465E10F2F-low.png Figure 4 Dev.ti.com Gallery

Once you’re in the Smart Analog Combo GUI, make sure to select Enable Function Generator Mode in the upper-right part of the screen. You are now set up to start using the demo.

What You Can Do with the Smart Analog Combo GUI

Using the Input Signal Source drop-down menu (Figure 5), you can select between the following options:

  • Internal DAC: Generate a signal from the 12-bit DAC, send to the PGA, and read using the 12-bit ADC.
  • P1.6 OA1 – Inverting PGA IN: Hook up a signal to pin 1.6 on the LaunchPad development kit and feed to the inverting PGA.
  • P1.7 OA1+ Non-Inverting PGA IN: Hook up a signal to pin 1.7 on the LaunchPad development kit and feed to the noninverting PGA.
  • P1.5 ADC Direct IN: Hook up a signal to pin 1.5 on the LaunchPad development kit directly to the 12-bit ADC.
GUID-052D5127-2711-46EC-9514-37CCFE637E55-low.png Figure 5 Input Signal Source Drop-down Menu

Generating a Signal Using the Internal 12-Bit DAC

Let’s try out the internal DAC drop-down option – there are two boxes. The top-left graph contains the signal generated by the DAC and the bottom-left graph is what the ADC measures. See Figure 6 below. By default, you should see the generation of a sine signal.

The block diagram below shows two smart analog combos in this configuration: one as the internal DAC and one as a PGA. Figure 6 also shows where the top-left graph is generating the signal and the bottom-left graph is measuring the signal.

GUID-79DC9E6B-97B0-4E1B-8D97-5C8E36BA1DFF-low.png Figure 6 Smart Analog Combo Modules Block Diagram

Let’s modify the waveform. In the DAC signal type box, select the SAWTOOTH waveform from the drop-down menu. Increase the signal frequency to 8Hz; you should now see the waveform shown in Figure 7 on the left side.

GUID-F6F45C60-6AD6-4CBD-B486-02FC49515EB9-low.png Figure 7 Sawtooth Inverting Waveform with a Signal Frequency = 8Hz

There are also options such as DAC frequency and signal amplitude. If you decrease the DAC frequency, you’ll notice the change in your waveform’s resolution. You can also change the signal amplitude through the DAC itself, or add an op-amp gain in the op-amp section.

If you switch the signal to noninverting and add a gain of 2, you will notice that the signal is now flipped and increased in amplitude, as shown in Figure 8.

GUID-4CCD2219-1371-4EBE-B08A-560D73130476-low.png Figure 8 Sawtooth Noninverting Waveform with Signal Frequency = 8Hz, Op-amp Gain = 2

You have now successfully run through all of the different options when generating an internal DAC signal on the Smart Analog Combo GUI. You can see that this GUI is a powerful tool with which you can evaluate the configurable analog on the MSP430FR2355. Grab an MSP430FR2355 LaunchPad development kit today. Learn more about the MSP430FR2355 MCU LaunchPad development kit.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale