• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Designing a Magnetically Immune Polyphase Smart Meter, Part 3: Comparing Isolated Shunt Sensing Architectures

    • SSZT600 october   2018 AMC1106M05 , AMC1210 , AMC1304M05 , ISO7731 , MSP430F67641A , MSP430I2041

       

  • CONTENTS
  • SEARCH
  • Designing a Magnetically Immune Polyphase Smart Meter, Part 3: Comparing Isolated Shunt Sensing Architectures
  1.   1
  2.   2
    1.     3
    2.     Metrology Calculations
    3.     Voltage Isolation
    4.     Interfacing to Host MCU
    5.     Data Rate
    6.     Solution Size and Crosstalk
    7.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Designing a Magnetically Immune Polyphase Smart Meter, Part 3: Comparing Isolated Shunt Sensing Architectures

Mekre Mesganaw

In part 1 of this three-part series, I discussed the isolated shunt sensing building blocks, and in part 2, I presented an overview of two different shunt sensing architectures. In this installment, I will compare the two architectures.

Figure 1 summarizes the differences between the isolated modulator and metrology analog front end (AFE) shunt sensing architectures.


GUID-0A4B2094-4597-4AFD-8648-241239C638B1-low.jpg

Figure 1 Comparing the Isolated Modulator and Metrology AFE Shunt Sensing Architectures

Metrology Calculations

In the isolated modulator architecture, the host/metrology microcontroller (MCU), not the isolated shunt sensing device, performs all metrology calculations. In the isolated metrology AFE architecture, the isolated shunt sensing device does the majority of calculations. This means that the isolated metrology AFE architecture offloads the work that the host MCU would otherwise do, which provides better separation between metrology and the host.

One disadvantage of this, however, is that since there isn’t one device with access to all of the raw analog-to-digital converter (ADC) data of the different phases, phase-to-phase calculations (such as determining the angle between different phase voltages) and advanced metrology analysis are more difficult with the isolated metrology AFE architecture compared to the isolated modulator architecture.

Voltage Isolation

One advantage of the isolated metrology AFE architecture is that it isolates both voltage and current since the isolated metrology AFE senses voltage in addition to current. In the isolated modulator architecture, voltage can only be isolated with additional circuitry.

Interfacing to Host MCU

An advantage of isolated modulator devices is that you do not have multiple devices sharing the same communication interface to the host MCU. If you’re using the AMC1210 stand-alone filter, then you only need to communicate to one AMC1210 device to get the current samples for as many as four channels. If you select an MCU with a digital filter, you can obtain the current ADC values directly from registers.

In comparison, when using the isolated metrology AFE architecture, you need to be able to share one universal asynchronous receiver transmitter (UART) receiver port of the host with three metrology AFEs, as shown in Figure 2.

GUID-74F0C1A2-72F0-4A62-88B3-7D5801F8CB1E-low.png Figure 2 Metrology AFE Reference Design UART Receiver Port Mapping Multiplexing Scheme

Data Rate

An advantage of the isolated metrology AFE architecture is that the rate at which data is sent is smaller than for the isolated modulator’s case. In the isolated metrology AFE design, data is sent out only once every second, with a baud rate of 57,600. For isolated modulator designs, the minimum data rate is 5-6MHz. The reduced data rate for the metrology AFE architecture means fewer issues with emissions.

Solution Size and Crosstalk

Another advantage of the isolated metrology AFE architecture is that it doesn’t require additional ADCs to sense the voltage like the isolated modulator architecture does. For the isolated modulator architecture, you would need to use at least a 10-bit ADC to sense the phase voltage, integrated within the host MCU. This would lead to the size of the isolated modulator designs being relatively larger than the isolated metrology AFE architecture.

However, one advantage of having the voltage sensed separately from the current is that there is less crosstalk from the voltage front-end circuitry to the current front-end circuitry. This voltage-to-current crosstalk is a factor in the energy percentage error seen at lower currents for the different architectures.

To summarize, the isolated modulator is good in systems that calculate advanced metrology parameters like harmonics and phase-to-phase measurements. The isolated metrology AFE architecture is good for low-emission, compact systems that require good separation of the metrology and host functions and only need basic metrology parameters calculated.

Additional Resources

  • View all TI smart e-meter reference designs.
  • Watch the Polyphase Current Measurement with Isolated Shunt Sensors training series.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale