• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Get Smart: How Intelligent Battery Gauges Improve Battery Life in Continuous Glucose Monitors

    • SSZT492 April   2019 BQ27421-G1 , BQ27426 , BQ27Z561-R1 , BQ2970 , BQ2971 , BQ2972 , BQ2973

       

  • CONTENTS
  • SEARCH
  • Get Smart: How Intelligent Battery Gauges Improve Battery Life in Continuous Glucose Monitors
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Get Smart: How Intelligent Battery Gauges Improve Battery Life in Continuous Glucose Monitors

Rushi Dalal

A high or a low blood glucose level in the body can cause serious health threats, so it makes monitoring glucose levels a high priority. And with more than 150 million people around the world with diabetes, the need for personal portable blood glucose monitors (BGMs) is great.

A continuous glucose monitor (CGM), shown in Figure 1, enables people with diabetes to check glucose readings in real time, or monitor glucose readings over an extended period of time. As the name implies, CGMs continuously monitor glucose levels and alert users of dangerous highs or lows. The monitor typically consists of a sensor unit, shown in Figure 2, and an aggregator unit, shown in Figure 3.

GUID-30771910-439B-4ADA-90AB-A7979BBF11A7-low.jpg Figure 1 A Cgm

The sensor unit connects to the body for a certain time period (eight to ten days, for instance). It uses a primary button-cell or coin-cell battery. The aggregator unit is a battery-powered handheld unit that harnesses radio-frequency (RF) technology such as Near Field Communication to read the glucose data. The battery-management subsystem of the aggregator unit comprises a battery charger, gauge and protection. A typical aggregator unit operates from a 3.7-V lithium-ion single-cell battery. It is rechargeable with either a USB or DC input from an adapter.

GUID-939E82BE-C528-48F2-BE54-C16DD6C852C4-low.jpg Figure 2 A CGM Sensor Unit
GUID-CCB7E844-17D8-4B15-BC3A-743646E84899-low.jpg Figure 3 Block Diagram of a CGM Aggregator Unit

Battery gauges help address critical battery-management problems by using predictive methods to estimate remaining battery capacity, state of charge, time to empty and state of health under various load conditions. By having intelligent battery gauging, you can extend the run time (as seen in Figure 4) and cycle life of the battery. TI’s Impedance Track™ gauging algorithm enables battery capacity predictability with >99% accuracy, and our battery gauges have superior analog measurement performance and battery characteristic modeling.

GUID-992BBC21-9295-4050-9AE3-D54C6965EB8A-low.jpg Figure 4 Extended Run Time with a TI Gauge

There are several single-cell gauging options that are compact, cost-effective and offer ultra-low power consumption. The fuel gauge can reside in the battery pack or system PCB, with the latter more common in portable medical applications.

Figure 5 and Figure 6 show typical system-side and pack-side gas-gauging configurations. Gauges on the system PCB such as the BQ27426 require minimal user configuration and consume little current during normal operation. For a higher level of integration, some gauges have an integrated sense resistor, like the BQ27421-G1.

On the other hand, if the gauge is designed into the battery pack, there are highly accurate options using flash-based firmware and integrated Secure Hash Algorithm-256 authentication, such as the BQ27Z561-R1. Protection integrated circuits, such as the BQ2970, can provide voltage, current and reverse charger protection.

GUID-27AC69F5-E796-48C7-B1DD-58ED9F60A5F9-low.jpg Figure 5 Typical Host/system-side Gas-gauging Configuration
GUID-E25CF8D9-4599-4B65-B2D1-9B872906CD11-low.jpg Figure 6 Typical Pack-side Gas-gauging Configuration

Battery gauges bring an increased level of sophistication and intelligence to power management. Systems without accurate gauges simply shut down at a fixed voltage. Many devices shut down at 3.5 V in order to cover worst-case reserve capacity (reserving battery energy for shutdown tasks), but as Figure 4 shows, simply measuring the battery voltage with a microcontroller and analog-to-digital converter to generate a low-battery warning is not a reliable method of gauging the remaining capacity, since most applications have variable load conditions. A battery gauge will compute the remaining capacity and alter the shutdown voltage to meet the reserve capacity under all conditions, in this case leading to increased run time.

In addition to the advantage of reserve capacity, some battery gauges have the ability to not report a 0% state of charge due to a high transient pulsed load from the application, causing the cell voltage to dip below the termination voltage. This is beneficial in cases where there is still significant capacity in the battery, but the high transient causes the termination voltage to be reached prematurely.

Batteries are complex electrochemical systems that are affected by battery aging, temperature and impedance. Algorithms, compact devices and advanced device integration are all key features in improving system performance. What are your biggest challenges in medical battery-operated applications like continuous blood glucose monitors? Tell us in the comments.

Additional Resources

  • Explore TI’s battery gauge portfolio.
  • Check out resources for blood glucose monitors.
  • Watch our “Battery Management Deep Dive On-Demand Technical Training.”
  • Read more blog posts about this topic:
    • “Why you should use a dedicated fuel gauge in your battery management system.”

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale