• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Optocouplers and Silicon-based Galvanic Isolation Technology – How Do They Work?

    • SSZT391 october   2019 ISO1211

       

  • CONTENTS
  • SEARCH
  • Optocouplers and Silicon-based Galvanic Isolation Technology – How Do They Work?
  1.   1
  2.   2
    1.     3
    2.     How does an optocoupler work?
    3.     How does a silicon-based isolator work?
    4.     Additional Resources:
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Optocouplers and Silicon-based Galvanic Isolation Technology – How Do They Work?

Galvanic isolation is a necessary form of protection for all electronics that interface with humans or other circuits against possible high-voltage events ranging from tens of volts to kilovolts. Isolation as a form of protection requires that communication between two circuits occurs through an insulation or isolation barrier, which prevents current from directly flowing between the circuits.

Over the past several decades, the technology used to isolate circuits has moved from optical-based to silicon-based – but how are these technologies really different?

How does an optocoupler work?

An optocoupler, as shown in Figure 1, consists of an input LED, a receiving photodetector and an output driver. The driver circuit and LED circuits are typically built using complementary metal-oxide semiconductor (CMOS) technology, with the insulation or isolation barrier usually consisting of molding compound. Both the input and output of an optocoupler isolator require separate voltage supplies connected through the anode and collector pins, and separate grounds typically connected at the cathode and emitter pins, in order to maintain signal isolation between the input and output.

GUID-E1785000-ED8F-4CCB-A88C-0E4A1060A1AA-low.jpg Figure 1 Optocoupler with pinout diagram

Communication within an optocoupler occurs when an applied CMOS logic input generates an input-side current, which then creates a proportional LED output for transmission through the molding compound barrier to the receiving photodetector and output.

The isolation performance of an optocoupler is determined by a combination of the LED, the molding compound used between the input and output, and the distance through the molding compound. Because the molding compound is a key contributor to isolation barrier strength, its quality plays a significant role in optocoupler lifetime, reliability and performance.

Standards bodies including Underwriters Laboratories (UL) and Verband der Elektrotechnik (VDE) determine optocoupler ratings, and those ratings specifically define the “distance through insulation” to accommodate molding compound variations during manufacture, along with partial discharge tests to identify molding compound defects that could compromise isolation performance under stress. Optocoupler standards have not historically included lifetime reliability performance data or high-voltage stress testing for sustained applied high voltages, and thus their sustained long-term performance and reliability can vary significantly.

How does a silicon-based isolator work?

Silicon-based isolation technology is based on CMOS technology, and consists of two separate integrated circuit (IC) chips – an input circuit and an output circuit – connected through bond-wires to enable data transfer, as shown in Figure 2.

GUID-FB59DC5C-CFAE-4345-AD55-AE9294E8A088-low.png Figure 2 Cross section of digital isolator construction

Both the input and output sides of the digital isolator, as shown in Figure 3, require separate voltage supplies (VCC1, VCC2) and separate grounds (GND1, GND2) to maintain signal isolation between the input and output.

Communication within a digital isolator occurs when applying a transistor-transistor logic or CMOS logic input to the digital input. The input signal is digitally translated into the frequency domain and then passed through a high-voltage capacitive barrier and across the connecting bond-wire to the receiving-side IC.

GUID-70201B48-3F20-4656-86A0-8A1035499544-low.png Figure 3 Digital isolator with pinout diagram

The insulator of a digital isolator circuit can be either a single or double silicon dioxide (SiO2) capacitive barrier, which can withstand extremely high voltages by design. Because the insulation barrier is constructed of high dielectric strength material (see Table 1) and is manufactured in a closely controlled wafer fab instead of an assembly line, part-to-part variation is unlikely, and the key contributors to isolation performance are the isolation technology and design. The white paper, "Enabling high voltage signal isolation quality and reliability," explores how this manufacturing process provides reliability, shock protection and reinforced isolation equivalent to two levels of basic isolation in a single package.

Table 1 Comparison of dielectrics
Insulator Materials Dielectric Strength
Air ~1 Vrms/μm
Epoxies ~20 Vrms/μm
Silica-filled mold compounds ~100 Vrms/μm
Polyimide ~300Vrms/μm
SiO2 ~500 Vrms/μm

The isolation ratings of silicon-based digital isolators are determined by a series of high-voltage tests defined through industry standards bodies such as UL, the International Electrotechnical Commission and VDE. The tests are the same as those for determining optocoupler ratings, as shown in Table 2, with additional high-voltage testing and material rating requirements. Because of the additional test conditions for high-voltage robustness and reliability, it is possible to publish lifetime reliability data.

Table 2 Comparison of optocoupler test conditions/digital isolator tests
Topic VDE 0884-11 Capacitive & Magnetic Digital Isolators IEC 60747-5-5 Optocouplers
Basic isolation Reinforced isolation Reinforced isolation only
1 Max surge isolation voltage VIOSM Test voltage = VIOSM x 1.3 Test voltage VIOSM x 1.6 Min 10 kV
Min. 10 kV
2 Partial discharge test voltage, VPD(M) 1.5 x VIORM 1.875 x VIORM 1.875 x VIORM
3 Working voltage, VIORM Based on TDDB analysis Based on TDDB analysis Based on PD test
4 Min. rated lifetime 20 years x 1.3 (security factor) 20 years x 1.875 (security factor Not defined
5 Failure rate over lifetime 1000 ppm 1 ppm Not defined
6 Allowed isolation materials SiO2 and thin film polymer SiO2 and thin film polymer Not limited

You should now have some insight into differences between optical isolation and silicon-based isolation performance, and the role of materials, manufacturing and even standards testing. While both optocoupler and silicon-based isolators are proven means of circuit protection, the real challenge in identifying the best isolation solution for your design will depend on your design objectives: reliability, lifetime and performance of the isolator all play a role in the right technology choice.

Additional Resources:

  • Explore how to easily upgrade from optocouplers to digital isolators in the application note, "How to Replace Optocouplers with Digital Isolators in Standard Interface Circuits."
  • Learn about the benefits of capacitive-based isolation for motor drive systems in the white paper, "How Capacitive Isolation Solves Key Challenges in AC Motor Drives."
  • For an in-depth overview of isolated digital inputs, read the article, "What are isolated digital inputs?".

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale