• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Exploring the Benefits of Multichannel Gate Drivers in Automotive Power Seats

    • SSZT086 march   2022 DRV8714-Q1 , DRV8718-Q1

       

  • CONTENTS
  • SEARCH
  • Exploring the Benefits of Multichannel Gate Drivers in Automotive Power Seats
  1.   1
  2.   2
    1.     3
    2.     Power-seat Design Trends
    3.     Multichannel Gate-driver Solutions
    4.     Drive Flexibility
    5.     Simplified Interface
    6.     Conclusion
    7.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Exploring the Benefits of Multichannel Gate Drivers in Automotive Power Seats

Clark Kinnaird

Unless you ride in a spacecraft, automotive power seats are probably the most complex chair in which you will ever sit. More adjustable than airplane seats – and much more comfortable than a dentist’s chair – automotive power seats provide a luxurious level of comfort, convenience and safety.

Whether you are moving the seat up and down, forward or backward, or adjusting lumbar support, motors make these maneuvers easy.  In addition to the advantage of ease of motion, highly-capable automotive power seats can have other advantages.  For example, it’s even possible for in-seat functions such as fans and heaters to extend vehicle range by reducing the power load on the whole-cabin temperature system.

Power-seat Design Trends

Given the amount of options in an automotive power seat, manufacturers are looking for ways to drive multiple motors. Designers have traditionally used relays to switch power to motors, but relays are comprised of several tiny mechanical parts and have limited speed capabilities. These disadvantages, plus the noise that relays make every time they switch, make them unsuitable for pulse-width modulation (PWM), which is used to control motor speeds.

One trend moves away from electromechanical relays to integrated circuits (IC) given the latter’s advantages, including smaller size, quiet operation, speed control and reliability. An IC’s fast, silent switching enables speed control using PWM to provide smooth movements and synchronized motion of multiple motors.

Relay-driven seats usually use only one relay for each motor, and the first IC designs followed that pattern. With only a few motors, the complexity penalty was tolerable. But combining the drive circuits for several motors in full-featured automotive seats offers significant benefits, including a reduction in the bill of materials and the smaller board space that results from a design approach using multi-axis integrated drivers.

Multichannel Gate-driver Solutions

TI offers multiple-motor automotive gate drivers designed for power seats. The DRV8714-Q1 and DRV8718-Q1 have four and eight channels, respectively, of half-bridge gate drivers. They integrate a charge pump, current-sense amplifiers and logic for multiple loads. One IC can control as many as seven different motors or a combination of motors and heaters, which reduces the number of necessary parts for a seat module.

Figure 1 shows the DRV8714-Q1 controlling three motors with shared half bridges. It is possible to operate any of the motors separately or run specific combinations simultaneously. You can select a metal-oxide semiconductor field-effect transistor (MOSFET) to best match the motor characteristics and adjust the registers of the DRV8714-Q1 to optimize performance.

GUID-6AD6C7AC-1473-46BF-A0F9-7EB3DB31526E-low.jpg Figure 1 A Three-motor Seat Driven by the DRV8714-Q1 Automotive Gate Driver

Drive Flexibility

With as many as eight channels of half-bridge drivers, the flexibility of the DRV8718-Q1 enables the driving of bidirectional motors, unidirectional motors (such as fans) and nonmotor loads such as heaters using the correct number of MOSFETs, each of which is tailored for the specific load.

Figure 2 shows a DRV8718-Q1 controlling four seat motors, plus a fan and a heater. The fan (which rotates in one direction) needs only one half bridge, and the heater requires only a high-side MOSFET, resulting in a design that reduces the number of external transistors – all because of the flexibility of the multichannel gate driver.

GUID-7533C431-F77A-46BF-A966-CE4490D1BB4E-low.jpg Figure 2 The DRV8718-Q1 Automotive Gate Driver Driving Motors, a Heater and a Fan

With the flexibility to choose each external MOSFET to best fit the corresponding load, it becomes possible to improve thermal performance in high-current applications using low drain-to-source on-resistance MOSFETs. The DRV8718-Q1 family facilitates improved electromagnetic compatibility by adjusting the gate current to control transition slew rates. You can also adapt your seat module to a variety of motors by changing the MOSFETs without altering the overall design.

Simplified Interface

Another advantage of a single chip is that you can significantly reduce the signals to the microcontroller (MCU). With only four pins (using Serial Peripheral Interface [SPI]), the MCU can control as many as eight half bridges with a single DRV8718-Q1, or even more channels in a daisy-chain configuration, as shown in Figure 3. This control includes setting the parameters for each half bridge, independent or coordinated control of the transistors, and diagnostic monitoring.

GUID-1F7D8C9A-26E7-4CBF-9BE9-512FEDF857DA-low.jpg Figure 3 Controlling 16 Half Bridges Using a Daisy-chain Configuration from the MCU to the DRV8718-Q1 Automotive Gate Driver

Unified control reduces the MCU’s workload. With one command, the MCU can enable all of the drives; with one register read, the MCU can tell if any of the motors have fault conditions. Subsequent SPI reads can determine the faulted channel and details if needed.

Conclusion

Automotive power seats continue to offer greater comfort and convenience. Driving their motors, however, presents several design challenges. Multichannel gate drivers help solve these challenges by integrating many channels into a single chip, along with features such as diagnostics and current-sense amplifiers. DRV8718-Q1 multichannel gate drivers provide a flexible, compact solution to accommodate the latest features of automotive seating.

Additional Resources

  • For more information about automotive power seats, see these technical articles:
    • "Putting Innovation in the Driver’s Seat. What Technologies Are Most Important to Modern Power Seats?"
    • "Why Are You Still Driving Automotive Motors With Relays?"
  • Check out the application note, "Relay Replacement for Brushed DC Motor Drive in Automotive Applications."
Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale