• Menu
  • Product
  • Email
  • PDF
  • Order now
  • 6 More Myths about Hall-effect Sensors

    • SSZT074 May   2022 TMAG5123 , TMAG5170

       

  • CONTENTS
  • SEARCH
  • 6 More Myths about Hall-effect Sensors
  1.   1
  2.   2
    1.     3
    2.     Myth No. 1: Only TMR Sensors Can Take In-plane Measurements.
    3.     Myth No. 2: Hall-effect Switches Are Not Useful Replacements for Reed Switches.
    4.     Myth No. 3: Hall-effect Sensors Are the Same as Hall Elements.
    5.     Myth No. 4: It Is Easy to Tamper with Systems Using Hall-effect Sensors.
    6.     Myth No. 5: Hall-effect Sensors Are Not Useful for Measuring Angles.
    7.     Myth No. 6: Linear Hall-effect Sensors Are Not Accurate.
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
6 More Myths about Hall-effect Sensors

Manny Soltero

Previously published on Electronic Design

In my previous Hall-effect sensor myths technical article, I focused on misconceptions about Hall-effect switches and latches, including common applications where designers could benefit from using Hall-effect sensors instead of other integrated circuits. The six myths in this article go a bit more in depth on the high-accuracy angle-measurement capabilities of Hall-effect sensors and their use in robotics systems for factory automation.

Myth No. 1: Only TMR Sensors Can Take In-plane Measurements.

Designers typically consider tunnel magneto-resistance (TMR) sensors because of their high magnetic sensitivity, high linearity and low power consumption. Plus, TMR sensors can sense magnetic fields horizontally (or in plane) with the package. Most Hall-effect sensors available today are sensitive to perpendicular fields, but there are a few, such as the TMAG5123, that have in-plane sensing capability. Figure 1 shows the sensitivity directionality of an in-plane sensor. See the application brief, "Sensing Magnetic Fields In-Plane Versus Out-of-Plane."

GUID-D51EC94B-6370-4C60-87AF-2BB5855C8C13-low.png Figure 1 In-plane Sensitivity

Myth No. 2: Hall-effect Switches Are Not Useful Replacements for Reed Switches.

Reed switches are still prevalent in many applications. Common reed-switch applications include door and window sensors. The main drawback of reed switches in security alarm systems is the inability to detect tampering events. By using a linear 3D Hall-effect sensor, designers can allocate any channel not used for active measurement to detect this event.

Another example is in a refrigerator door to control the exact position, where the inside light is turned on or off. Hall-effect switches offer consistent open-and-close distance detection given their tight threshold hysteresis specifications.

Another major drawback of reed switches is their inability to use standard printed circuit board (PCB) assembly procedures. These switches must be hand-soldered onto the board, thus complicating the assembly process and increasing costs. Table 1 compares the two technologies.

Table 1 Comparison of Hall-effect Switches and Reed Switches
Specifications Hall-effect switches Reed switches
Magnet orientation sensitivity Orthogonal and in plane Parallel (same as in plane)
Current draw Microampere range (low-frequency duty cycle) Microampere to milliampere range (pulsed by microcontroller [MCU] general-purpose input/output)
Polarity sensitivity Both poles (omnipolar) Both poles
Hysteresis Single-digit millitesla range 40%-95% variation
Switch loads directly? Requires additional circuitry Yes (up to 3 A)
Response time ≅10 µs 25 µs to 100 µs
Life expectancy Effectively unlimited operations – limited by silicon life expectancy From thousands to billions of operations depending on load
Shock susceptibility None Yes
Assembly Standard PCB assembly Manual assembly with high yield loss (10%)
Operating temperature –40°C to 125°C –55°C to 200°C

Myth No. 3: Hall-effect Sensors Are the Same as Hall Elements.

It is not true that Hall elements are essentially the same as Hall-effect sensors. The Hall element, which requires bias circuitry and a differential amplifier, is the most basic structure needed to produce a usable voltage. In contrast to Hall-effect sensors, Hall elements do not have all supporting circuitry integrated into a single package.

Figure 2 shows the circuit implementation for both types of sensors. Hall elements are typically used for applications where accuracy is not critical, cost is of extreme importance, and a differential amplifier is nearby to minimize external noise coupling. Additionally, Hall elements have an inherent nonlinear variation over temperature, while Hall-effect sensors have built-in compensation to ensure stable measurements across a wide temperature range of –40°C to 125°C. For more information about Hall-effect sensors, see the article, "What is a Hall-effect sensor?"

GUID-1BFABF83-93B4-48D6-85DE-B25C0AD8079A-low.png Figure 2 Circuit Implementation for a Hall Element (a) versus a Hall-effect Sensor (b)

Myth No. 4: It Is Easy to Tamper with Systems Using Hall-effect Sensors.

It is possible to tamper with systems using reed switches and basic Hall-effect switches – this is true. Large external magnetic fields can trick a system such that it functions as if everything is working properly. A good way to fix this is to use a linear 3D Hall-effect sensor. One axis monitors the presence of the intended magnet, while the other two channels detect external magnetic fields. Using a linear 3D sensor with a configurable magnetic threshold per channel provides more flexibility in setting the proper "tamper detection" threshold. The example in Figure 3 shows an MCU receiving an interrupt signal once the threshold is crossed.

GUID-0AABD4D5-CCA4-40FF-924F-392B158FD65B-low.jpg Figure 3 Tamper Detection Using a Linear 3D Hall-effect Sensor

Myth No. 5: Hall-effect Sensors Are Not Useful for Measuring Angles.

Hall-effect sensors are popular in many displacement applications, but they are also used for absolute angle measurements. By strategically positioning two single-axis linear Hall-effect sensors around a rotating dipole magnet, each sensor picks up a magnetic field vector that is out of phase with the other. With this information, it is easy to calculate the exact angle of the rotating magnet by using the arctangent function.

Figure 4a shows two implementations using linear sensors in two different package types. A more elegant way to perform angle measurement is with a single linear 3D Hall-effect sensor (see Figure 4b for various configurations). To learn about angle measurements, read "Absolute Angle Measurements for Rotational Motion Using Hall-Effect Sensors" and "Angle Measurement With Multi-Axis Linear Hall-Effect Sensors."

GUID-3F6796EE-E561-460E-9396-47EEF74F99A4-low.png Figure 4 Absolute Angle Measurement Using Two Single-axis Linear Hall-effect Sensors (a) and One Linear 3D Hall-effect Sensor (b)

Myth No. 6: Linear Hall-effect Sensors Are Not Accurate.

Linear Hall-effect sensors are cost-effective solutions that provide reliable magnetic information. Users of such sensors know this fact, but often consider other technologies to meet their high-accuracy requirements. For example, industrial robot arms must be precisely positioned in relation to their target object(s), and using a high-accuracy linear 3D Hall-effect sensor such as the TMAG5170 provides the precision needed for these applications (Figure 5). Additionally, both the high precision and low-sensitivity drift over temperature of the TMAG5170 potentially eliminate the need for system-level calibration.

GUID-3F4E1FB0-8E92-4F45-B4C1-C3EA5D86BB04-low.png Figure 5 A Linear 3D Sensor in a Robotic Arm Application

I hope you have enjoyed my articles debunking commonly held myths about Hall-effect sensors. These sensors continue to gain popularity in automotive and industrial applications through their high accuracy and increasing variety of integrated functions and diagnostics.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale