• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Increasing Surgical Drill Trigger Precision and Control with Inductive and Hall-effect Sensors

    • SSZT060 october   2022 LDC3114

       

  • CONTENTS
  • SEARCH
  • Increasing Surgical Drill Trigger Precision and Control with Inductive and Hall-effect Sensors
  1.   1
  2.   2
    1.     3
    2.     Hall-effect Sensors for Linear Displacement in Variable-speed Triggers for Surgical Drills
    3.     Inductive Sensors for Contactless Surgical Drill Triggers
    4.     Conclusion
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Increasing Surgical Drill Trigger Precision and Control with Inductive and Hall-effect Sensors

Christen Waite

Surgical drills are controlled either by a trigger, similar to the control on a power drill, or a foot pedal. In the past, most surgical drills used mechanical triggers. But because of their contact-based operation, these devices can wear out over time; as a result, the accuracy of the speed control can decline.

Designers are now seeking a contactless alternative to mechanical triggers while still providing accurate speed control measurements.

The input user interface subsystems of the surgical drill block diagram shown in Figure 1 represent the trigger for speed control and other user-initiated functionalities. In a contactless trigger design, Hall-effect sensors measure the linear displacement of the trigger to help control the drill speed, while inductive sensors create hermetically sealed touch-button controls that can indicate whether the drill is properly gripped when in operation.

GUID-D4D721C3-3147-40F9-92F1-52C53EF21E9D-low.png Figure 1 High-level Block Diagram of a Surgical Drill

Hall-effect Sensors for Linear Displacement in Variable-speed Triggers for Surgical Drills

Let’s discuss how to implement a contactless, variable-speed trigger with a single-axis (one-dimensional) linear Hall-effect sensor with an analog output. Outputting a varying voltage that depends on how far the trigger is pressed enables more accurate speed control compared to a mechanical trigger that uses a potentiometer to translate the displacement position of the trigger to an output voltage that adjusts its speed based on pre-set speed settings. Potentiometers rely on contact-based operation and typically wear down faster than noncontact-based alternatives, especially if the potentiometer is exposed to vibrations or other environmental factors such as moisture and debris. This approach reduces wear and tear compared to traditional mechanical-based triggers and is possible for both trigger- and pedal-controlled drills.

Another benefit of using a contactless trigger design, is the option to use low-power Hall-effect switches along with a load switch to keep the system in a low-power standby mode when not pressed. As outlined in the Contactless Hall-Effect Variable-Speed Trigger Reference Design with External Field Protection, you can also implement an optional magnetic field protection feature to prevent external magnetic fields from influencing the speed control. Figure 2 shows an implementation of this reference design in 3D-printed mechanical housing to create a complete contactless trigger system.

GUID-B1862A63-E5BE-4378-B588-BA3AECBCB33D-low.png Figure 2 TI’s evaluation module for a Contactless Hall-effect Variable-speed Trigger with External Field Protection

Inductive Sensors for Contactless Surgical Drill Triggers

In addition to reliable and accurate operation, enhanced safety features are also a consideration when designing surgical drills. Since traditional surgical drills are mechanically controlled, the drill could be unintentionally enabled by accidentally stepping on the pedal or pressing the trigger. Placing a guard around the trigger or pedal can help to avoid accidental operation, but does not provide protection electronically.

Inductive sensors can help solve this challenge by implementing safety features designed to prevent unintentional operation of the equipment. Figure 3 shows an example of the placement of sensor coils on either side of the handle to detect whether the user is properly gripping the drill; If not, the drill will not turn on. This approach is effective for both foot-pedal and trigger-operated drills.

GUID-0FBC19B3-C198-40B0-B775-31E6B6F09B27-low.jpg Figure 3 Example of Sensor Coil Placement for Grip Detection

It is also possible to use inductive sensors for touch buttons on the drill to control settings and features, such as the direction of the motor. Some inductive sensors, such as TI’s LDC3114, have an integrated button algorithm or allow access to raw data representing the measured inductance value, which provides flexibility for how to use the device. This raw data can differentiate between a normal button push and a press and hold or force touch action, facilitating the ability for a single button to support multiple actions that could be used for device feature selection, instead of just supporting a binary output. For example, a regular button press could put the drill into oscillation mode while pressing and holding the button could put the drill into a slow-motion mode.

Unlike mechanical buttons that require cutouts that are difficult to seal, you can place inductive sensors behind flat surfaces that can be hermetically sealed, such as a sheet of metal or plastic, making sterilization easier between uses than traditional mechanical buttons. Using an inductive sensing touch button provides a more reliable solution that uses the slight deflection of the flat surface being pressed to determine a button press instead of relying on a mechanical connection. This approach, as demonstrated in the Inductive Touch and Magnetic Dial Contactless User Interface Reference Design, allows the use of a many as eight touch buttons with gloves, which are commonly present in medical settings, while ignoring environmental factors like debris or damage to the button surface.

Conclusion

Hall-effect and inductive sensors are more reliable for contactless trigger and button designs then traditional contact-based designs because they will be less likely to wear and tear over time due to environmental factors, such as the sterilization process for surgical equipment. Contactless trigger designs do not completely eliminate mechanical elements, such as the spring to give the trigger a resistive feel, but a contactless trigger design minimizes the number of potential points subjected to frequent wear and tear. Using the increased precision and reliability of sensors allows doctors to have more confidence their surgical tools without worrying about accuracy declining over time.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale