• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How to Design an Intelligent Battery Junction Box for Advanced EV Battery Management Systems

    • SSZT047 january   2023 BQ79616-Q1 , BQ79631-Q1 , BQ79731-Q1

       

  • CONTENTS
  • SEARCH
  • How to Design an Intelligent Battery Junction Box for Advanced EV Battery Management Systems
  1.   1
  2.   2
    1.     3
    2.     Voltage, Temperature and Current Measurement
    3.     Over Current Fault Detection and Protection
    4.     Voltage and Current Synchronization
    5.     Synchronization Requirements
    6.     Remote Device Communication Support
    7.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

How to Design an Intelligent Battery Junction Box for Advanced EV Battery Management Systems

Issac Hsu

As electric vehicles (EVs) become more popular, the challenge for automakers is to reflect true range while making the vehicle more affordable. This translates into making the battery packs lower cost with higher energy densities. Every single watt-hour stored and retrieved from the cells is critical to extend the driving range.

The main function of a battery management system (BMS) is to monitor cell voltages, pack voltages and pack current. In addition, due to the high-voltage design of the BMS, insulation resistance measurement between the high-voltage domain and low-voltage domain is needed in order to catch defects in the battery structure and protect against hazardous conditions.

GUID-34E42F3F-412E-4E81-8619-BE7CEC0ABC4F-low.png Figure 1 A Traditional BMS Architecture (a);
a BMS Architecture with an Intelligent Battery Junction Box (BJB) (b)

Figure 1 presents a typical BMS architecture containing a battery management unit (BMU), cell supervisor unit (CMU) and a battery junction box (BJB). A BMU typically has a microcontroller (MCU), which manages all of the functions within the battery pack. The traditional BJB is a relay box or a switch box with power contactors that connects the entire battery pack to the load inverter, motor or the battery charger.

Figure 1a shows the traditional BMS. There are no active electronics inside of the junction box. All of the measurements in the BJB are measured at the BMU. There are wires connecting the BJB into the analog-to-digital converter (ADC) terminals.

Figure 1b shows the intelligent BJB. There is a dedicated pack monitor inside the box that measures all voltages and currents and passes the information to the MCU using simple twisted-pair communication. It helps eliminating wires and cabling harnesses; and improves voltage and current measurements with lower noise.

Voltage, Temperature and Current Measurement

Figure 2 shows the different high voltages, current and temperatures that the pack monitor measures inside a BJB enabled by the BQ79731-Q1 battery pack monitor.

GUID-59F0297A-6830-435A-A1E3-087E0503766E-low.png Figure 2 High-voltage Measurements inside the BJB
  • Voltage: The high-voltage is measured using divided-down resistor strings. These voltage measurements monitor the state of high-voltage components in the system.
  • Temperature: The temperature measurements monitor the temperature of the shunt resistor so that the MCU can apply compensation, as well as the temperature of the contactors to make sure that they are not stressed beyond the normal operating conditions.
  • Current: The current measurements are based on either:
    • A shunt resistor - Because the currents in an EV can go up to thousands of amperes, the shunt resistance values are extremely small – in the range of 25 µOhms to 50 µOhms; or
    • A Hall-effect sensor – Used to measure the EV current on the high-voltage rail, while still being isolated. Its dynamic range is typically limited, thus there can be multiple sensors in the system to measure the entire range.

Over Current Fault Detection and Protection

Detection and prevention of an over-current even is required in a BMS in order to prevent catastrophic damage that can occur to the battery pack in the event of a short circuit, exposed high-voltage terminal or defective equipment. An over current circuit integrated in the BJB unit will use the current sense information measured through either the shunt resistor or hall-effect sensor and the battery pack monitor. This measurement is then processed and compared to a threshold inside the battery pack monitor while the same has the capability of signaling an over-current event through dedicated outputs which will be used to enable a fuse-driver in order to blow the high-voltage separator (pyro-fuse). Since the reaction time for this needs to be as fast as possible, a dedicated signal processing path is implemented in the battery pack monitor device.

Voltage and Current Synchronization

Voltage and current synchronization is the time delay that exists to sample the voltage and current between the pack monitor and cell monitor. These measurements are mainly used for calculating state of charge and state of health through electro-impedance spectroscopy (EIS). Calculating the impedance of the cell by measuring the voltage, current and power across the cell enables the BMS to monitor the instantaneous power of the car.

The cell voltage, pack voltage and pack current have to be time-synchronized to provide the most accurate power and impedance estimations. Taking samples within a certain time interval is called the synchronization interval. The smaller the synchronization interval, the more accurate the power estimate or the impedance estimate. The more accurate the state-of-charge estimation, the more accurate remaining mileage drivers get.

Synchronization Requirements

Next-generation BMS will require synchronized voltage and current measurements in less than 1 ms, but there are the challenges in meeting this requirement:

TI’s battery monitors can maintain a time relationship by issuing an ADC start command to the cell monitor and the pack monitor. These battery monitors also support delayed ADC sampling to compensate for the propagation delay when transmitting the ADC start command down the daisy-chain interface.

Remote Device Communication Support

Another benefit of the intelligent BJB is the streamlined data communication by using the versatile daisy-chain interface not just for battery pack and battery cell monitor devices, but also remote devices like EEPROM memory or any type of sensors that are placed in the modules with different physical placement in the vehicle. In this case the pack and monitor device also act as an interface translator offering I2C or SPI data to be transferred through the daisy-chain interface which eliminates wires and cabling harnesses and in turn reduces the overall EV weight.

The massive electrification efforts happening in the automotive industry are driving the need to reduce the complexity of BMS by adding electronics in the junction box, while enhancing system safety. A pack monitor can locally measure the voltages before and after the relays, the current through the battery pack. The accuracy improvements in voltage and current measurements will directly result in optimal utilization of a battery. The BQ79631-Q1 and BQ79731-Q1 from TI can optimize the performance and reduce the future cost of intelligent BJBs by integrating all necessary functions of the system in a single device. Effective voltage and current synchronization enable precise state-of-health, state-of-charge and EIS calculations that will result in optimal utilization of the battery.

In addition, TI’s BQ79616-Q1 and BQ79718-Q1battery cell monitor families offer accurate cell voltage and temperature measurements as a part of the CSU implementation which enables a complete BMS eco-system.

Additional Resources

  • Watch these TI training videos:
    • “Intelligent Battery Junction Box for Voltage and Current Synchronization.”
    • “xEV Battery Pack Autonomous Management in Park Mode.”
  • Check out the white paper, “Functional Safety Considerations in Battery Management for Vehicle Electrification.”

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale