• Menu
  • Product
  • Email
  • PDF
  • Order now
  • AM263x Sitara™ Microcontroller Silicon Revision 1.0A, 1.1

    • SPRZ488E March   2022  – May 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1

       

  • CONTENTS
  • SEARCH
  • AM263x Sitara™ Microcontroller Silicon Revision 1.0A, 1.1
  1.   1
  2. 1Usage Notes and Advisories Matrices
  3. 2Silicon Usage Notes
    1.     i2324
    2.     i2348
    3.     i2364
  4. 3Silicon Advisories
    1.     i2310
    2.     i2311
    3.     i2313
    4.     i2329
    5.     i2345
    6.     i2346
    7.     i2347
    8.     i2349
    9.     i2350
    10.     i2352
    11.     i2353
    12.     i2354
    13.     i2355
    14.     i2356
    15.     i2357
    16.     i2358
    17.     i2359
    18.     i2374
    19.     i2375
    20.     i2386
    21.     i2392
    22.     i2393
    23.     i2394
    24.     i2395
    25.     i2401
    26.     i2402
    27.     i2403
    28.     i2404
    29.     i2405
    30.     i2427
    31.     i2428
    32.     i2433
    33.     i2438
    34.     i2439
  5.   Trademarks
  6. 4Revision History
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

Errata

AM263x Sitara™ Microcontroller
Silicon Revision 1.0A, 1.1

1 Usage Notes and Advisories Matrices

Table 1-1 lists all usage notes and the applicable silicon revision(s). Table 1-2 lists all advisories, modules affected, and the applicable silicon revision(s).

Table 1-1 Usage Notes Matrix
Module DESCRIPTION SILICON REVISIONS AFFECTED
AM263x
1.0A 1.1
CLOCKS i2324 — No synchronizer present between GCM and GCD status signals YES
YES
QSPI i2364 — QSPI: Access to address beyond 8MB is not supported in mem map mode YES YES
VDDA i2348 — VDDA1V8 Static Power leakage YES
NO
Table 1-2 Advisories Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM263x
1.0A 1.1
ADC i2346 — ADC result has Error when switching between odd and even channels YES
NO
ADC i2347 — VREF current consumption of ADC is random at powerup YES
NO
ADC i2349 — ADC VrefHi Loading increase in powerdown YES NO
CONTROLSS i2352 — CONTROLSS-SDFM: Dynamically Changing Threshold Settings (LLT, HLT), Filter Type, or COSR Settings Will Trigger Spurious Comparator Events YES YES
CONTROLSS i2353 — CONTROLSS-SDFM: Dynamically Changing Data Filter Settings (Such as Filter Type or DOSR) Will Trigger Spurious Data Acknowledge Events YES YES
CONTROLSS i2354 — CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events YES YES
CONTROLSS i2355 — CONTROLSS-ADC: DMA Read of Stale Result YES YES
CONTROLSS i2356 — CONTROLSS-ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set YES YES
CONTROLSS i2357 — CONTROLSS-ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the End of the Blanking Window YES YES
CONTROLSS i2358 — CONTROLSS-ePWM: Trip Events Will Not be Filtered by the Blanking Window for the First 3 Cycles After the Start of a Blanking YES YES
CONTROLSS i2359 — CONTROLSS-CMPSS:Prescaler counter behavior different from spec when DACSOURCE is made 0 or reconfigured as 1 YES YES
CONTROLSS i2405 — CONTROLSS: Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss YES YES
CPSW i2345 — CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks YES YES
CPSW i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES YES
CPSW i2402 — CPSW: Ethernet to Host Checksum Offload does not work YES YES
CPSW i2438 — CPSW - Host to Ethernet Checksum Generation with VLAN ADD/Remove YES YES
CPSW i2439 — CPSW: Host to Ethernet Timestamp Accuracy Issue YES YES
CRC i2386 — CRC: CRC 8-bit data width and CRC8-SAE-J1850 and CRC8-H2F possible use in CAN module is not supported YES YES
DCC i2395 — DCC Module Frequency Comparison can Report Erroneous Results YES YES
GPMC i2313 — GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO YES YES
M4 ROM i2403 — M4 ROM: SBL redundant boot image feature not supported on HSSE devices NO YES
MBOX i2404 — MBOX: Race condition in mailbox registers resulting in events miss YES YES
McSPI i2350 — McSPI data transfer using EDMA in ‘ABSYNC’ mode stops after 32 bits transfer YES YES
MDIO i2329 — MDIO interface corruption (CPSW and PRU-ICSS) YES NO
PBIST i2374 — PBIST fails if clock frequency of R5SS_CORE_CLK is not same as R5FSS_CLK_SELECTED frequency YES YES
SOC CONTROL i2392 — Race condition in mem-init capture registers resulting in events miss YES YES
BUS SAFETY i2393 — Granular error status not logged in BUS_SAFETY_ERR registers for the detected faults YES YES
SOC CONTROL i2394 — Race condition in interrupt and error aggregator capture registers resulting in events miss YES YES
SFDM i2375 — SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected YES YES
UART i2310 — USART: Erroneous triggering of timeout interrupt YES YES
UART i2311 — USART: Spurious DMA Interrupts YES YES
RAM SEC i2427 — RAM SEC can cause Spurious RAM writes resulting in L2 & MBOX memory corruption YES YES
AES i2428 — AES in DTHE generates extra dma request for data_in at the end of GCM encrypt YES YES
ICSS i2433 — ICSS: Reading the 64-bit IEP timer does not have a lock MSW logic when LSW is read YES YES
CPSW i2438 — CPSW: Host to Ethernet Checksum Generation with VLAN ADD/Remove YES YES
CPSW i2439 — CPSW: Host to Ethernet Timestamp Accuracy Issue YES YES

2 Silicon Usage Notes

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale