• Menu
  • Product
  • Email
  • PDF
  • Order now
  • How Radar is Displacing Traditional Technologies

    • SPRY346 March   2022 AWR1843 , AWR1843AOP , AWR2243 , AWR2944

       

  • CONTENTS
  • SEARCH
  • How Radar is Displacing Traditional Technologies
  1.   At a glance
  2.   Authors
  3.   Introduction
  4.   Advancing from 24-GHz to 77-GHz radar for mid- and short-range applications
  5.   Imaging radar vs. lidar
  6.   Expanding radar to new applications
  7.   Radar for ultra-short-range applications
  8.   Driver monitoring for ADAS
  9.   Conclusion
  10. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

MARKETING WHITE PAPER

How Radar is Displacing Traditional Technologies

At a glance

1 Introduction
Understand how radar has positively impacted safety and efficiency within the automotive industry.
2 Advancing from 24-GHz to 77-GHz radar for mid- and short-range applications
Explore why the market is moving towards higher resolution and smaller size, 77-Ghz mmWave radar sensors for mid- and short-range applications.
3 Imaging radar vs. lidar
Learn how an imaging radar’s ability can be used to differentiate design and provide a cost-effective high-resolution sensor.
4 Expanding radar to new applications
Examine why today’s automakers and Tier-1 suppliers turn to radar mmWave sensors for ADAS applications such as parking and driver monitoring.

Authors

Prajakta Desai
Marketing Manager for Automotive Radar
Texas Instruments

Introduction

As the level of autonomy in cars increases, choosing the right number and type of sensors becomes more complex. Traditional sensing options are available, but over the years, the application of radar within the automotive industry has positively evolved the definition of safety and efficiency.

Because it can work in extreme environmental conditions such as rain, snow, dust and bright sunlight and also provide precise distance and velocity information, radar is considered the most appropriate sensing modality to meet New Car Assessment Program (NCAP) requirements. Vehicle architectures are increasingly relying on smart radar sensors, with all processing occurring at the edge to send object lists to central electronic control units.

Radar sensing has become a cost-efficient sensing modality for required advanced driver assistance system (ADAS) functions and to meet Society for Automotive Engineers vehicle autonomy levels 2+ and even 3+, as shown in Figure 1. Radar technology is evolving to support higher levels of automated driving, with high levels of range and resolution for precise detection and decision. And because radar sensors can now support multiple functions, the use of space around the vehicle becomes more manageable. As the numbers of sensors increase, the space around the car becomes constrained. Due to multimodal functionally of the sensors, engineers are eventually able reduce the number of sensors.

Figure 1 Radar sensors enable advanced levels of autonomy.

Up to level 3+, vision and radar sensing modalities can cost efficiently address the requirements, while for level 4 and beyond, all three sensing modalities – including lidar – might be necessary (as shown in Table 1). Radar sensors, when built with cascaded transceivers (a higher number of virtual channels), offer lidar-like performance (higher angular resolution), but at an optimized cost.

Table 1 Autonomy levels and their corresponding sensing requirements.
Level 2+
5 sensors
Front:
1 short range
1 medium range
Rear:
1 short range
1 medium range
1 long range
Level 3+
7 or more sensors
All of the sensors named above for front and rear
Plus sensors on each side of the car for 360° coverage
Level 4 and beyond
All sensing modalities
Front: Short- and medium-range sensors
Rear: Short-, medium- and long-range sensors
Sides: May include all sensing modalities including cameras, radar and lidar

Radar technology alerts drivers to the possibility of a collision by providing a warning or taking necessary evasive action. The complexity of safely turning or changing lanes and navigating tight corners presents significant design challenges when working to advance vehicle autonomy, however. Visibility around corners has presented major technical barriers in designing high-quality ADAS and parking assistance, as well as affecting the broader adoption of autonomous vehicles worldwide. Being able to see farther and more clearly with radar devices leads to improved sensor fusion for safer automated driving and parking applications. In addition to the performance that radar brings to the table, the key advantage of using radar for ADAS is its ability to operate reliably regardless of weather conditions.

77- to 81-GHz millimeter-wave (mmWave) long-range radar sensors from TI offer the ability to detect objects in a wide geographical area and can cover a range of 200 m. Mid-range sensors operate in the range of 100 m to 150 m, while short-range sensors use transceivers, with signal-processing equipment mounted behind the bumper, to track an object or person 30 m to 50 m from the vehicle. Complementary metal-oxide-semiconductor technology has enabled a high level of integration in our front end, especially a single chip that integrates both analog and digital.

Advancing from 24-GHz to 77-GHz radar for mid- and short-range applications

For short-range radar, the 24-GHz narrow and ultrawide bands have been used in legacy automotive sensors. For simple applications such as basic blind-spot detection, you can use the industrial, scientific and medical (ISM) band, but in most cases, including ultra-short-range radar applications, the need for high-range resolution dictates use of the ultrawide band. This 24-GHz ultra-wide band will be phased out soon, however, given spectrum regulations and standards developed by the European Telecommunications Standards Institute and the U.S. Federal Communications Commission. The 24-GHz ultra-wide band became unavailable as of January 1, 2022, known as the “sunset date,” in both Europe and the U.S.; only the narrow ISM band will be available in the long term. The lack of wide bandwidth in the 24-GHz band, coupled with the need for higher performance in emerging radar applications, makes 24 GHz unattractive for new short-range radar implementations.

There is a 76- to 77-GHz band available for vehicular long- and mid-range radar applications. This band has the benefit of high allowed equivalent isotropic radiated power, which enables front long-range radar applications such as adaptive cruise control. The 77- to 81-GHz short-range radar band has recently gained significant traction, both from a worldwide regulation perspective as well as industry adoption.

One of the key benefits of 77 GHz frequency band for automotive is its wide bandwidth. Compared to the 200-MHz ISM band, which is available at 24 GHz, the 77- to 81-GHz short-range radar band offers up to 4 GHz of sweep bandwidth, significantly improving range resolution and accuracy. The range resolution of a radar sensor signifies its ability to separate two closely spaced objects, whereas the range accuracy represents the accuracy in measuring the distance of a single object. Since range resolution and accuracy are inversely proportional to the sweep bandwidth, a 77-GHz radar sensor can achieve 20 times better performance in range resolution and accuracy compared to 24-GHz radar. The achievable range resolution is 4 cm (versus 75 cm for 24-GHz radar) as shown in Figure 2. Because the 24-GHz band will be restricted to narrow bandwidth, moving forward, most 24-GHz automotive radar sensors will likely shift to the 77-GHz band.

Figure 2 77-GHz Wide bandwidth with provides higher range resolution and accuracy.

Smaller sensor size is another advantage of a higher radio frequency. For a chosen antenna field of view and gain, the size of the antenna array can be approximately three times smaller each in the X and Y dimensions when comparing 77 GHz to 24 GHz (see Figure 3). This size reduction is particularly useful in the context of automotive applications (where sensors need to be mounted in tight spots behind the bumper); in other spots around the car, including doors and trunks for some proximity applications; and inside the car for in-cabin applications.

Figure 3 The 77-GHz antenna array is significantly smaller than the 24-GHz antenna array.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale