• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPSM365R6V3EVM User’s Guide

    • SNVU846 December   2022

       

  • CONTENTS
  • SEARCH
  • TPSM365R6V3EVM User’s Guide
  1.   Abstract
  2.   Trademarks
  3. 1Setup
    1. 1.1 Test Points
    2. 1.2 Jumpers
  4. 2Operation
    1. 2.1 Quick Start
  5. 3Schematic
  6. 4Board Layout
  7. 5Bill of Materials
  8. 6Typical Characteristics
  9. 7Application Curves
  10. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

EVM USER'S GUIDE

TPSM365R6V3EVM User’s Guide

1 Abstract

The TPSM365R6V3EVM evaluation board (EVM) allows for evaluation of TPSM365R6, a synchronous step-down DC/DC module capable of driving up to 0.6-A of load current from a wide input voltage of up to 65-V. This EVM is configured to provide a 3.3V fixed output voltage. The switching frequency is set to 1MHz, and can also be synced to an external signal. The EVM can also serve as an example for circuit layout and design for a user's end application. See the TPSM365R6, 3-V to 65-V Input, 600-mA, 4-μA No-Load IQ Synchronous Buck Converter Power Module in a HotRod™ QFN Package data sheet for additional features, detailed descriptions, and available options.

Table 1-1 Device and Package Configurations
EVMU1FREQUENCYSPREAD SPECTRUMCURRENTPIN 11 TRIM

TPSM365R6V3EVM

TPSM365R6V3RDNR

Fixed (1MHz)

Disabled0.6 AMODE/SYNC
TPSM365R6V3EVM Board

Trademarks

HotRod™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 Setup

Figure 1-1 shows a typical setup with the EVM. The VIN power terminal block (J1) is used for connection to the host input supply and the VOUT power terminal block (J4) is used for connection to the load.

1.1 Test Points

The test points on the top of the board can be used for connecting to the input and output of the EVM. Table 1-1 describes each test point.

Table 1-1 Test Point Descriptions
Test Point(1)Description
VINS+Sense line for measuring the input voltage. Not meant to be used to power the device.
VINS-Ground test point located near the ground terminal of the high frequency bypass capacitor. Meant to be connected to the ground sense line for VIN, but can be used in place of a general ground test point.
VOUTS+Sense line test point for the output voltage. Do not connect to an output load.
VOUTS-Ground test point located near the ground terminal of the output capacitors. Meant to be connected to the ground sense line for VOUT, but can be used in place of a general ground test point.
GNDTest points for ground connection. Not meant to be used as a ground connection for the input power supply.
ENInput voltage scope monitor. Connect an oscilloscope probe to this set of points to measure input ripple voltage.
PGOODThis test point is connected to the PGOOD pin from the IC. This test point is an open-drain output of the PGOOD pin. In this EVM configuration, the pin is pulled up to VOUT by R4.
ENThis test point is connected to the EN pin. By default, there is a pullup resistor R2 (RENT) to VIN to enable the IC.
SYNCThis test point is connected to the RT pin of the IC when the R4 (RMODE) is installed. In a MODE/SYNC trimmed part, this test point is connected to the SYNC pin of the IC. This can be connected to an external clock to synchronize the IC. In a MODE/SYNC configuration, make sure J6 is configured to the SYNC setting in order to hookup to an external clock signal.
VCCThis test point is connected to the VCC pin.
(1) Refer to the product data sheet for absolute maximum ratings associated with the features in this table.

Figure 1-1 EVM Board Connections

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale