SNVA966 July 2020 – MONTH LP8864-Q1 , LP8864S-Q1 , LP8866-Q1 , LP8866S-Q1
All other trademarks are the property of their respective owners.
The LP8864-Q1, LP8864S-Q1, LP8866-Q1, and LP8866S-Q1 (hereafter, LP886XX-Q1) devices have a huge variety of fault detections and diagnostic features. The system could make use of all these features to better evaluate the current system condition, making the most suitable decision. It will help to avoid both overacting under minor faults and underacting under critical faults.
However, to fully leverage all those features, a well-organized fault handling routine is needed. The following figure is the recommended software handling routine which works with the LP886XX-Q1 devices.
When a fault is detected through the FAULT pin, the software needs to take related action.
Faults can be resolved in the following ways by the fault handling routine:
Higher critical level actions are taken if current level actions do not solve the issue. The details of those specific actions are described in Section 2. The corresponding system-level action to handle faults and incorrect diagnostic information will differ based on different faults detected.