• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Component Temperature Monitoring Using Differential Temperature Measurements

    • SNIA044 November   2021 TMP61 , TMP61-Q1 , TMP63 , TMP63-Q1 , TMP64 , TMP64-Q1

       

  • CONTENTS
  • SEARCH
  • Component Temperature Monitoring Using Differential Temperature Measurements
  1.   Trademarks
  2. 1Introduction
  3. 2Component Temperature Monitoring With Adjacent PCB Placement
  4. 3Component Temperature Monitoring Using Differential Techniques
    1. 3.1 Physics of Differential Temperature Measurements
    2. 3.2 Three-Point Differential Temperature Measurement
    3. 3.3 Differential Temperature Measurement Design Guidelines
      1. 3.3.1 Example: Differential Temperature Layout for a Power IC
  5. 4Summary
  6. 5References
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Component Temperature Monitoring Using Differential Temperature Measurements

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

When monitoring the temperature of critical components in a system, better accuracy leads to better information feedback to temperature control loops used for compensation or safety shutdown purposes. In some ICs, designers include a thermal diode pin, which connects to an external temperature sensor to monitor the internal temperature of the die. This method is viable when the internal diode-connected transistor used for temperature sensing is well-constructed and has an overtemperature behavior which closely follows that of a standard BJT.

Some ICs may not have an internal thermal transistor designed in, or its overtemperature characteristics may provide poor quality for temperature detection. Instead, the designer may choose to use the internal temperature sensor of the device if one is available. One main disadvantage of the included temperature sensing element in most ICs is that they have extremely low accuracy—typically on the order of ± 5°C to 10°C—because process deviation in silicon can be 15% or more, which leads to high temperature errors in the die.

There are several options for measuring the temperature of the desired component. Option 1 is to use the internal diode or temperature sensor, if available. Option 2 is to place an external integrated temperature sensor or thermistor on the PCB as close as possible to the heat source. Finally, option 3 is to calculate the temperature of the component by taking differential temperature measurements. Option 3 enables highly-accurate temperature monitoring using a dedicated thermal layout (for example, a ground plane, heat sink, or dedicated thermal trace) and two temperature sensors, such as TI’s TMP6 thermistors.

2 Component Temperature Monitoring With Adjacent PCB Placement

The most common method of monitoring the temperature of a critical component is to place a temperature sensor directly next to the component. Heat conducts to the sensor via the PCB and traces. This method is cheap and simple, but thermal interference from ambient temperature and heat from other components on the board affect the temperature sensor. The heat radiated from the critical component can also decay very quickly, especially when the temperature differential between the component and ambient is very high. Figure 2-1 shows a thermal capture of the AWR2243BOOST evaluation module (EVM) mounted onto the DCA1000EVM for data capture. The HI temperature reading shows that the AWR2243, operating at a moderate load, has reached a temperature of 51.5°C. The LO value is the ambient temperature of 22.9°C, and the board temperature as measured by the thermal camera is 41.9°C.

GUID-20210923-SS0I-GHPR-1D7N-RLKCV3LQHKG3-low.png Figure 2-1 Thermal Capture of AWR2243BOOST Under Moderate Load

As shown, the quality of temperature data declines as distance from the radar chip on the PCB increases. By placing a temperature sensor adjacent to the AWR2243, the measured temperature even a few centimeters away from the heat source will be several degrees Celsius less than the actual die temperature of the device. This is due to the various thermal resistances between the component and the location of the temperature sensor.

Furthermore, there are often temperature gradients on the die blocks of the chips themselves. When monitoring critical components, it is important to accurately monitor the temperature of the precise hot spot of the device, which can be difficult if using only one adjacent external temperature sensor.

Finally, Figure 2-2 shows a thermal simulation of a test board with a temperature sensor near a 100°C heat source. The temperature at the temperature sensor is significantly lower than the temperature of the heat source due to the thermal resistances between the two. There are techniques to compensate for these thermal resistances and estimate the die temperature from one external temperature measurement, but the exact thermal resistances are difficult or even impossible to determine, making it difficult to accurately measure the die temperature of the device across a wide temperature range.

GUID-20210923-SS0I-8QTB-WDSP-FRRDJVBDKQVZ-low.png Figure 2-2 Thermal Simulation of Temperature Sensor Near 100°C Heat Source

From the examples provided, it is evident that a different technique is necessary to accurately monitor the temperature of certain components using external sensors. One effective technique is to use differential temperature measurements.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale