• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPS7H4001-SP Worst Case Analysis Model

    • SLVUC15 March   2021 TPS7H4001-SP

       

  • CONTENTS
  • SEARCH
  • TPS7H4001-SP Worst Case Analysis Model
  1.   1
  2.   2
    1.     3
    2.     4
  3.   5
    1.     6
    2.     7
  4.   8
    1.     9
    2.     10
  5. IMPORTANT NOTICE
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
USER'S GUIDE

TPS7H4001-SP Worst Case Analysis Model

Trademarks

Pspice are registered trademarks of Cadence.

All trademarks are the property of their respective owners.

1 TPS7H4001-SP WCA Model Specification

The TPS7H4001-SP WCA model is a behavioral model intended for simulation of frequency response characteristics, such as phase margin, phase margin crossover frequency, and gain margin. Monte Carlo analysis can also be performed to observe the distribution of behavior across a specified sample size of devices. The following sources of variation are incorporated into the model:

    Process Device-to-device manufacturing differences
    Temperature Over full military range: -55°C to 125°C
    Load Up to the maximum recommended load: 18 A
    Radiation Up to the maximum rated Total Ionizing Dose (TID) of the device: 100 krad
    Aging

    Represented by data taken at 25°C before and after 1,000 hours of testing at 125°C, and meant to emulate 15 years operating at 65-95°C as defined by Group C specifications in MIL-PRF-38535

In the model, the specific device parameters influenced by the above variation include:

    gmea Error amplifier transconductance
    gmps Power stage transconductance
    VREF Reference voltage

1.1 Model Parameters

The following parameters are used within the model to define the internal characteristics, operating environment, and configuration of the device.

Parameter Description Default Model Value
Mean_GMea The mean value of the error amplifier transconductance 1800 µS
Mean_GMps The mean value of the power stage transconductance 40 S
Mean_Vref The mean value of the reference voltage 0.605 V
Tol_GMea The tolerance of the error amplifier transconductance [1] 8.72 %
Tol_GMps The tolerance of the power stage transconductance [1] 5.22 %
Tol_Vref The tolerance of the reference voltage [1] 0.31 %
TID The Total Ionizing Dose the device is subjected to, within the range of 0 to 100 krad 0 krad
AGING

Binary value indicating the presence of aging effects, where:

0 = No aging effects added

1 = Aging effects added

0

L Output inductor value 0.9 µF
FS Switching frequency 500 kHz
TEMP Operating temperature, which is set within the simulation profile and takes the default value unless otherwise specified. 27°C

[1] For Gaussian distributions, tolerance is defined as the standard deviation (1-sigma) divided by the mean and is expressed as a percentage.

In addition to the listed model parameters, external component selection will also influence device behavior. The external components used in the default schematic take nominal values and, as such, users may see fit to add tolerances to them to model real-world variation.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale