• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Transient Response Comparison of AECM with D-CAP2 and PCM Control

    • SLVAFD5 December   2022 TPS562211 , TPS562212 , TPS563211 , TPS563212

       

  • CONTENTS
  • SEARCH
  • Transient Response Comparison of AECM with D-CAP2 and PCM Control
  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 PCM
    2. 1.2 DCAP2
    3. 1.3 AECM
  4. 2Transient Response Comparison
  5. 3Summary
  6. 4References
  7. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Transient Response Comparison of AECM with D-CAP2 and PCM Control

Abstract

The output voltage transient of a buck regulator during a load current step is often a key performance specification, which is the response characteristic to a sudden load fluctuation, that is, the time until the output voltage returns to a preset value after having fallen or risen, and the waveform of the output voltage. While there are many types of control topologies addressing special design challenges for non-isolated DC/DC converter, including peak current mode control, constant on-time (COT) control, D-CAP2™ control mode (a variation of adaptive constant-on time control mode), advanced emulated current mode (AECM). The various control modes each has unique advantages. This note, we will provide a performance comparison of DC/DC converters operating in three different modes: PCM control mode, D-CAP2™ control mode (a derivative of constant on-time), and AECM control mode. These three control modes were all used widespread, none of these control modes require loop compensation which making the design simple.

Trademarks

D-CAP2™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 Introduction

The output voltage transient of a buck regulator during a load current step is often a key performance specification.While there are many types of control topologies addressing special design challenges for non-isolated DC/DC converter, including Voltage-mode control, peak current mode control, constant on-time (COT) control, D-CAP2 control mode a variation of adaptive constant-on time control mode, advanced emulated current mode (AECM).

No single control topology is a good fit for all applications. The various control modes each has unique advantages. This note, we will provide a performance comparison of DC/DC converters operating in three different modes: PCM control mode, D-CAP2™ control mode (a derivative of constant on-time), and AECM control mode. These three control modes were all used widespread, none of these control modes require loop compensation which making the design simple.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale