• Menu
  • Product
  • Email
  • PDF
  • Order now
  • TPSI3050-Q1 Change List

    • SLVAF73 November   2021 TPSI3050-Q1

       

  • CONTENTS
  • SEARCH
  • TPSI3050-Q1 Change List
  1.   Trademarks
  2. 1Introduction
  3. 2Errata Details
  4. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

TPSI3050-Q1 Change List

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

The TPSI3050-Q1 is a fully integrated isolated switch driver, which when combined with an external power switch, forms a complete isolated solid state relay solution. With a nominal gate drive voltage of 10 V 1.5-A peak source current and 3-A peak sink current, a large variety of external power switches can be chosen to meet a wide range of applications.

2 Errata Details

The following summarizes known errata.

Table 2-1 PTPSI3050QDWZRQ1 Errata Summary
Errata Number Description
1 In two-wire mode, under some conditions, the falling edge of EN can not be recognized, leading to VDRV being asserted low after a duration of tHL_VDRV_PD.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale